2020-03-13 10:57 PM
Thank you for helping.
environment
STM32CubeIDE Ver1.3.0
STM32CubeMx Ver5.6.0
TouchGFX Ver4.13.0
board
STM32F769I-DISCO
The project made with TouchGFX was started with STM32CubeIDE.
Open STM32F769I_DISCO.ioc and select LWIP from category
Enabled cannot be checked in Mode.
Why?
Can TouchGFX and LwIP be used at the same time?
Thank you.
Solved! Go to Solution.
2020-04-03 1:23 AM
Hi @Ebun.1 ,
Just Enable ETH ,then the Enable Lwip can be checked ,it is a condition for being able to access LWIP.
Best Regards,
Khouloud
2020-03-14 8:43 AM
Have a look at this http://ausleuchtung.ch/stm32-nucleo-f767zi-web-server/
It is not STM32F769 , but F767ZI. Still it is the F7 programmed with STM32CubeIDE Ver1.3.0.
2020-03-14 3:10 PM
Thank you for your reply.
It seems that what you introduce has nothing to do with TouchGFX.
2020-03-14 3:22 PM
You both should be warned about the "quality" of ST's code:
2020-03-14 5:19 PM
Thank you for your reply.
Does that mean there is a defect?
Are they deadly?
2020-03-22 9:36 PM
Are you unable of reading even the title and the first sentence?
2020-03-25 3:10 AM
Hello @Ebun.1 ,
Could you please share your ioc file ?
Best Regards,
Khouloud
2020-04-02 11:39 PM
2020-04-03 1:23 AM
Hi @Ebun.1 ,
Just Enable ETH ,then the Enable Lwip can be checked ,it is a condition for being able to access LWIP.
Best Regards,
Khouloud
2020-04-05 9:08 PM
�?�返事�?�り�?��?��?��?��?��?��?��?�。
�?�?�り�?��?�。
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.