2020-07-29 10:39 PM
Hi @Martin KJELDSEN
I just updated to 4.14.0. Now I get the linker as I got them in this thread (the problem was the short enums/wchar settings) https://community.st.com/s/question/0D50X0000AlgbG2SQI/arm6-compiler-support
I can see that the armclang lib that comes with 4.14.0 is smaller than the version you provided in the thread.
Any thoughts?
Cheers /jimmii
Solved! Go to Solution.
2021-11-01 2:56 AM
Hello Martin,
could you please provide a library for TouchGFX 4.18 for the Clang Compiler 6 by arm for the Cortex M7 processor with the compiler option short enum/wchar. Only then I can use the middleware of arm together with TouchGFX.
Thanks in advance
2021-11-01 7:34 AM
2021-11-02 12:28 AM
Hello Romain,
thanks for the library. I tried to compile my project. With the new library I get the following error message:
.\Objects\TouchTest1.axf: Error: L6218E: Undefined symbol touchgfx::HAL::blitCopyGlyph(unsigned char const*, unsigned short, unsigned short, unsigned short, unsigned short, unsigned short, touchgfx::colortype, unsigned char, touchgfx::BlitOperations) (referred from touchgfxgeneratedhal.o).
.\Objects\TouchTest1.axf: Error: L6218E: Undefined symbol touchgfx::HAL::blitCopyARGB8888(unsigned short const*, unsigned short, unsigned short, unsigned short, unsigned short, unsigned short, unsigned char) (referred from touchgfxgeneratedhal.o).
.\Objects\TouchTest1.axf: Error: L6218E: Undefined symbol touchgfx::HAL::blitCopy(unsigned short const*, unsigned char const*, unsigned short, unsigned short, unsigned short, unsigned short, unsigned short, unsigned char, bool, unsigned short, touchgfx::Bitmap::BitmapFormat, touchgfx::Bitmap::BitmapFormat) (referred from touchgfxgeneratedhal.o).
.\Objects\TouchTest1.axf: Error: L6218E: Undefined symbol touchgfx::HAL::blitCopy(unsigned short const*, unsigned short, unsigned short, unsigned short, unsigned short, unsigned short, unsigned char, bool) (referred from touchgfxgeneratedhal.o).
.\Objects\TouchTest1.axf: Error: L6218E: Undefined symbol touchgfx::HAL::blitCopy(unsigned short const*, unsigned short, unsigned short, unsigned short, unsigned short, unsigned short, unsigned char, bool, unsigned short, touchgfx::Bitmap::BitmapFormat, touchgfx::Bitmap::BitmapFormat) (referred from touchgfxgeneratedhal.o).
.\Objects\TouchTest1.axf: Error: L6218E: Undefined symbol touchgfx::HAL::blitFill(touchgfx::colortype, unsigned short, unsigned short, unsigned short, unsigned short, unsigned char) (referred from touchgfxgeneratedhal.o).
.\Objects\TouchTest1.axf: Error: L6218E: Undefined symbol touchgfx::HAL::blitFill(touchgfx::colortype, unsigned short, unsigned short, unsigned short, unsigned short, unsigned char, unsigned short, touchgfx::Bitmap::BitmapFormat) (referred from touchgfxgeneratedhal.o).
Do I need to include additional files in my MDK project in version 4.18? The same error message appears when I use the provided library without (short enums/wchar).
Regards
Ferdinand
2021-11-08 2:29 AM
Hello Romain,
my problem occurred because I upgraded the project from 4.17 to 4.18. I have set up the project again as a 4.18 project. After that I was able to compile everything without errors.
Thanks again for the library.
/Ferdinand
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.