2019-05-23 11:09 PM
2019-05-24 4:31 AM
Hi @ananya,
Do you have any more information to share about this? Build logs? Thanks
/Martin
2019-06-02 10:23 PM
The error was..
Error[Li005]: no definition for "touchgfx::InternalFlashFont::InternalFlashFont(touchgfx::GlyphNode const *, unsigned short, unsigned short, unsigned char, unsigned
char, unsigned char, unsigned char, unsigned char const *, touchgfx::KerningNode const *, unsigned short, unsigned short)" [referenced from C:\TouchGFXProjects\
MyApplication17\target\IAR\Debug\Obj\FontGetters.o]
Error[Li005]: no definition for "touchgfx::LockFreeDMA_Queue::LockFreeDMA_Queue(touchgfx::BlitOp *, unsigned long)" [referenced from C:\TouchGFXProjects\
MyApplication17\target\IAR\Debug\Obj\STM32F4DMA.o]
Error[Li005]: no definition for "Virtual function table for touchgfx::LCD16bpp" [referenced from C:\TouchGFXProjects\MyApplication17\target\IAR\Debug\Obj\
BoardConfiguration.o]
Error[Li005]: no definition for "touchgfx::HAL::setMCUActive(bool)" [referenced from C:\TouchGFXProjects\MyApplication17\target\IAR\Debug\Obj\OSWrappers.o]
Error[Li005]: no definition for "touchgfx::HAL::instance" [referenced from C:\TouchGFXProjects\MyApplication17\target\IAR\Debug\Obj\OSWrappers.o]
Error[Li005]: no definition for "touchgfx::HAL::initialize()" [referenced from C:\TouchGFXProjects\MyApplication17\target\IAR\Debug\Obj\BoardConfiguration.o]
Error[Li005]: no definition for "touchgfx::Bitmap::registerBitmapDatabase(touchgfx::Bitmap::BitmapData const *, unsigned short, unsigned short *, unsigned int,
unsigned int)" [referenced from C:\TouchGFXProjects\MyApplication17\target\IAR\Debug\Obj\BoardConfiguration.o]
Error[Li005]: no definition for "touchgfx::FontManager::setFontProvider(touchgfx::FontProvider *)" [referenced from C:\TouchGFXProjects\MyApplication17\target\IAR\
Debug\Obj\BoardConfiguration.o]
Error[Li005]: no definition for "touchgfx::Application::getInstance()" [referenced from C:\TouchGFXProjects\MyApplication17\target\IAR\Debug\Obj\
BoardConfiguration.o]
Error[Li005]: no definition for "touchgfx::TypedText::texts" [referenced from C:\TouchGFXProjects\MyApplication17\target\IAR\Debug\Obj\BoardConfiguration.o]
Error[Li005]: no definition for "touchgfx::AbstractPartition::~AbstractPartition() [subobject]" [referenced from C:\TouchGFXProjects\MyApplication17\target\IAR\Debug\
Obj\BoardConfiguration.o]
Error[Li005]: no definition for "touchgfx::AbstractPartition::AbstractPartition() [subobject]" [referenced from C:\TouchGFXProjects\MyApplication17\target\IAR\Debug\
Obj\BoardConfiguration.o]
Error[Li005]: no definition for "touchgfx::Application::clearAllTimerWidgets()" [referenced from C:\TouchGFXProjects\MyApplication17\target\IAR\Debug\Obj\
FrontendApplicationBase.o]
Error[Li005]: no definition for "touchgfx::Screen::bindTransition(touchgfx::Transition &)" [referenced from C:\TouchGFXProjects\MyApplication17\target\IAR\Debug\
Obj\FrontendApplicationBase.o]
Error[Li005]: no definition for "touchgfx::HAL::DISPLAY_HEIGHT" [referenced from C:\TouchGFXProjects\MyApplication17\target\IAR\Debug\Obj\Screen1View.o]
Error[Li005]: no definition for "touchgfx::HAL::DISPLAY_WIDTH" [referenced from C:\TouchGFXProjects\MyApplication17\target\IAR\Debug\Obj\Screen1View.o]
Error[Li005]: no definition for "touchgfx::Screen::Screen() [subobject]" [referenced from C:\TouchGFXProjects\MyApplication17\target\IAR\Debug\Obj\
Screen1ViewBase.o]
Error[Li005]: no definition for "touchgfx::Image::setBitmap(touchgfx::Bitmap const &)" [referenced from C:\TouchGFXProjects\MyApplication17\target\IAR\Debug\Obj\
Screen1ViewBase.o]
Error[Li005]: no definition for "touchgfx::ButtonWithLabel::ButtonWithLabel()" [referenced from C:\TouchGFXProjects\MyApplication17\target\IAR\Debug\Obj\
Screen1ViewBase.o]
Error[Li005]: no definition for "touchgfx::Color::getColorFrom24BitRGB(unsigned char, unsigned char, unsigned char)" [referenced from C:\TouchGFXProjects\
MyApplication17\target\IAR\Debug\Obj\Screen1ViewBase.o]
Error[Li005]: no definition for "touchgfx::AnimatedImage::setBitmaps(unsigned short, unsigned short)" [referenced from C:\TouchGFXProjects\MyApplication17\target\
IAR\Debug\Obj\Screen1ViewBase.o]
Error[Li005]: no definition for "touchgfx::AnimatedImage::setUpdateTicksInterval(unsigned char)" [referenced from C:\TouchGFXProjects\MyApplication17\target\IAR\
Debug\Obj\Screen1ViewBase.o]
Error[Li005]: no definition for "touchgfx::Button::setBitmaps(touchgfx::Bitmap const &, touchgfx::Bitmap const &)" [referenced from C:\TouchGFXProjects\
MyApplication17\target\IAR\Debug\Obj\Screen1ViewBase.o]
Error[Li005]: no definition for "touchgfx::Container::add(touchgfx::Drawable &)" [referenced from C:\TouchGFXProjects\MyApplication17\target\IAR\Debug\Obj\
Screen1ViewBase.o]
Error[Li005]: no definition for "touchgfx::TypedText::typedTexts" [referenced from C:\TouchGFXProjects\MyApplication17\target\IAR\Debug\Obj\
Screen1ViewBase.o]
Error[Li005]: no definition for "touchgfx::TypedText::numberOfTypedTexts" [referenced from C:\TouchGFXProjects\MyApplication17\target\IAR\Debug\Obj\
Screen1ViewBase.o]
Error[Li005]: no definition for "touchgfx::TypedText::fonts" [referenced from C:\TouchGFXProjects\MyApplication17\target\IAR\Debug\Obj\Screen1ViewBase.o]
Error[Li005]: no definition for "touchgfx::AnimatedImage::startAnimation(bool const &, bool const &, bool const &)" [referenced from C:\TouchGFXProjects\
MyApplication17\target\IAR\Debug\Obj\Screen1ViewBase.o]
Error[Li005]: no definition for "touchgfx::AnimatedImage::pauseAnimation()" [referenced from C:\TouchGFXProjects\MyApplication17\target\IAR\Debug\Obj\
Screen1ViewBase.o]
Error[Li005]: no definition for "Virtual function table for touchgfx::Image" [referenced from C:\TouchGFXProjects\MyApplication17\target\IAR\Debug\Obj\
Screen1ViewBase.o]
Error[Li005]: no definition for "Virtual function table for touchgfx::AnimatedImage" [referenced from C:\TouchGFXProjects\MyApplication17\target\IAR\Debug\Obj\
Screen1ViewBase.o]
Error[Li005]: no definition for "Virtual function table for touchgfx::Box" [referenced from C:\TouchGFXProjects\MyApplication17\target\IAR\Debug\Obj\
Screen1ViewBase.o]
Error[Li005]: no definition for "touchgfx::Application::currentScreen" [referenced from C:\TouchGFXProjects\MyApplication17\target\IAR\Debug\Obj\
FrontendApplicationBase.o]
Error[Li005]: no definition for "touchgfx::Application::currentTransition" [referenced from C:\TouchGFXProjects\MyApplication17\target\IAR\Debug\Obj\
FrontendApplicationBase.o]
Error[Li005]: no definition for "touchgfx::Application::draw()" [referenced from C:\TouchGFXProjects\MyApplication17\target\IAR\Debug\Obj\
FrontendApplicationBase.o]
Error[Li005]: no definition for "touchgfx::Application::Application() [subobject]" [referenced from C:\TouchGFXProjects\MyApplication17\target\IAR\Debug\Obj\
FrontendApplicationBase.o]
Error[Li005]: no definition for "touchgfx::Application::instance" [referenced from C:\TouchGFXProjects\MyApplication17\target\IAR\Debug\Obj\
FrontendApplicationBase.o]
Error[Li005]: no definition for "touchgfx::HAL::taskEntry()" [referenced from C:\TouchGFXProjects\MyApplication17\target\IAR\Debug\Obj\main.o]
Error[Li005]: no definition for "touchgfx::HAL::registerEventListener(touchgfx::UIEventListener &)" [referenced from C:\TouchGFXProjects\MyApplication17\target\IAR\
Debug\Obj\BoardConfiguration.o]
Error[Li005]: no definition for "touchgfx::HAL::USE_DOUBLE_BUFFERING" [referenced from C:\TouchGFXProjects\MyApplication17\target\IAR\Debug\Obj\
STM32F4HAL.o]
Error[Li005]: no definition for "touchgfx::HAL::USE_ANIMATION_STORAGE" [referenced from C:\TouchGFXProjects\MyApplication17\target\IAR\Debug\Obj\
STM32F4HAL.o]
Error[Li005]: no definition for "touchgfx::HAL::DISPLAY_ROTATION" [referenced from C:\TouchGFXProjects\MyApplication17\target\IAR\Debug\Obj\
BoardConfiguration.o]
Error[Li005]: no definition for "touchgfx::HAL::FRAME_BUFFER_WIDTH" [referenced from C:\TouchGFXProjects\MyApplication17\target\IAR\Debug\Obj\
BoardConfiguration.o]
Error[Li005]: no definition for "touchgfx::HAL::FRAME_BUFFER_HEIGHT" [referenced from C:\TouchGFXProjects\MyApplication17\target\IAR\Debug\Obj\
BoardConfiguration.o]
Error[Li005]: no definition for "touchgfx::DMA_Interface::executeCompleted()" [referenced from C:\TouchGFXProjects\MyApplication17\target\IAR\Debug\Obj\
STM32F4DMA.o]
Error[Li005]: no definition for "touchgfx::HAL::swapFrameBuffers()" [referenced from C:\TouchGFXProjects\MyApplication17\target\IAR\Debug\Obj\STM32F4HAL.o]
Error[Li005]: no definition for "touchgfx::HAL::allowDMATransfers()" [referenced from C:\TouchGFXProjects\MyApplication17\target\IAR\Debug\Obj\STM32F4HAL.o]
Error while running Linker
2019-06-03 1:42 AM
This looks like IAR, yea?
It looks like your application is not linking with the touchgfx library. Can you check your linker settings?
/Martin
2019-06-11 12:59 AM
Any update on this @ananya ?
2019-06-19 12:29 AM
Yes i Checked with linker settings and it is working.
2019-06-19 12:39 AM
Ok, that's great!
/Martin
2019-06-19 11:12 PM
Hi Martin,
I have another query.
I'm creating numeric keyboard. How to take input from the buttons to a buffer of text area??
2019-06-20 12:26 AM
Hi Anaya,
There are a few ways of going about creating a keyboard.
1) Just use standard buttons. In this case, you have a reference to the button and you can deduce what was pressed and which number to write into your wildcard buffer (displayed by your text area).
2) Use a "map" where you simply create a container and have one touch handler for the whole area, inspecting the coordinates to evaluate what was pressed. In this case you'll just have a Rect mapped to a number.
Does that make sense?
/Martin
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.