2020-11-17 7:30 AM
Hello,
Still developping on my STM32H753VT6 with touchGFX. Instead of loading images with touchGFX designer, I want to decode a JPEG image and then display it on my LCD screen.
For the moment I've just checked the example for the STM32H750B-DK demo board. It is obviously working on the demo board but not on my MCU. Indeed I'm stucked at this point :
/*##-4- Wait till end of JPEG decoding #*/
while(Jpeg_HWDecodingEnd == 0)
{
}This means that my decoding never finishes.
However I think i've added all the code to make the JPEG decoder working. Here is what i've added :
In main.c file :
#include "decode_dma.h"
#include "image_320_240_jpg.h"
JPEG_HandleTypeDef hjpeg;
JPEG_ConfTypeDef JPEG_Info;
uint32_t image_320_240_jpg_decoded[] = {0};
extern const unsigned char image_320_240_jpg[];
extern uint32_t Jpeg_HWDecodingEnd;
static void MX_JPEG_Init(void);
hjpeg.Instance = JPEG;
volatile HAL_StatusTypeDef res = HAL_JPEG_Init(&hjpeg);
JPEG_Decode_DMA(&hjpeg, (uint32_t) image_320_240_jpg1, IMAGE_320_240_JPG_SIZE, (uint32_t) image_320_240_jpg_decoded);
/*##-4- Wait till end of JPEG decoding #*/
while(Jpeg_HWDecodingEnd == 0)
{
}
/*##-5- Get JPEG Info ###############################################*/
HAL_JPEG_GetInfo(&hjpeg, &JPEG_Info);
/**
* @brief JPEG Initialization Function
* @param None
* @retval None
*/
static void MX_JPEG_Init(void)
{
/* USER CODE BEGIN JPEG_Init 0 */
/* USER CODE END JPEG_Init 0 */
/* USER CODE BEGIN JPEG_Init 1 */
/* USER CODE END JPEG_Init 1 */
hjpeg.Instance = JPEG;
if (HAL_JPEG_Init(&hjpeg) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN JPEG_Init 2 */
/* USER CODE END JPEG_Init 2 */
}
In stm32h7xx_hal_msp.c file :
HAL_JPEG_MspInit and HAL_JPEG_MspDeInit functions
In stm32h7xx_it.c file :
/**
* @brief This function handles JPEG interrupt request.
* @param None
* @retval None
*/
void JPEG_IRQHandler(void)
{
HAL_JPEG_IRQHandler(&hjpeg);
}
/**
* @brief This function handles MDMA interrupt request.
* @param None
* @retval None
*/
void MDMA_IRQHandler()
{
/* Check the interrupt and clear flag */
HAL_MDMA_IRQHandler(hjpeg.hdmain);
HAL_MDMA_IRQHandler(hjpeg.hdmaout);
}and in it's header file :
void MDMA_IRQHandler(void);
void JPEG_IRQHandler(void);decode_dma.h and decode_dma.c files have also been added
I've attached the example project.
If someone knows where the problem may come from, it would be a pleasure to see the answer !
Best regards,
AJT141
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.