2025-05-05 2:26 AM
I have two buttons (up and down) that moves by one step the scroll wheel using the function animateToItem
It seems, but I may be wrong, that UpdateCenterItem is not called when animateToItem, is executed Is it correct?
Solved! Go to Solution.
2025-05-05 5:05 AM
@GaetanGodart wrote:I am not sure what is "UpdateCenterItem".
Per your documentation is the function that it's called specifically for the item currently selected on the scroll wheel
@GaetanGodart wrote:However, when calling animateToItem, the elements gets updated to show the correct information.
yes, I can confirm that, however if I use in the code the animateToItem(x) the visualization correctly shows the item x as the selected item but, it seems it does not trigger the UpdateCenterItem
Anyway, I've just figured out that the function "is therefore only generated if the usage of a Selected Style Template is selected." which I hadn't selected.
Turning on Selected Style Template made the function animateToItem work
2025-05-05 3:51 AM
Hello @nico23 ,
I am not sure what is "UpdateCenterItem".
However, when calling animateToItem, the elements gets updated to show the correct information.
Is it not what you experienced?
Regards,
2025-05-05 5:05 AM
@GaetanGodart wrote:I am not sure what is "UpdateCenterItem".
Per your documentation is the function that it's called specifically for the item currently selected on the scroll wheel
@GaetanGodart wrote:However, when calling animateToItem, the elements gets updated to show the correct information.
yes, I can confirm that, however if I use in the code the animateToItem(x) the visualization correctly shows the item x as the selected item but, it seems it does not trigger the UpdateCenterItem
Anyway, I've just figured out that the function "is therefore only generated if the usage of a Selected Style Template is selected." which I hadn't selected.
Turning on Selected Style Template made the function animateToItem work
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.