2020-12-21 3:31 AM
Hi,
I've developed a UI with touchGFX where I'm using a swipe container and to finish my application I think I need a way to know the page I was in the Swipe container.
The steps I do are.:
1) in page x of the swipe container i press a button to go to another screen
2) when I'm in the other screen I press a button on a keyboard to come back to the previous screen and I need to come back exactly to the page of the Swipe container I was before.
I've read some discussion on the community about that but If I've understood well, the only way is to add manually a custom container. But I'm at the end of the UI so I would prefer to not follow this way. Is this the only way?
So far I've tried to add this function to SwipeContainer.cpp but I got errrors:
uint8_t SwipeContainer::getSelectedPage()
{
return currentPage;
}
and to SwipeContainer.hpp (in the public part)
uint8_t getSelectedPage();
In the screen where the swipe container is used:
uint8_t Screen01View::SaveCurrentPage()
{
currentPage=SwipeFunction.getSelectedPage();
return currentPage;
}
In the hpp file :
uint8_t SaveCurrentPage();
The error that appears is that one:
Compiling simulator/main.cpp
Linking build/bin/simulator.exe
build/MINGW32_NT-6.2/gui/src/screen01_screen/Screen01View.o: In function `ZN12Screen01View15SaveCurrentPageEv':
C:.......TouchGFX/gui/src/screen01_screen/Screen01View.cpp:581: undefined reference to `touchgfx::SwipeContainer::getSelectedPage()'
collect2.exe: error: ld returned 1 exit status
generated/simulator/gcc/Makefile:154: recipe for target 'build/bin/simulator.exe' failed
make[2]: *** [build/bin/simulator.exe] Error 1
make[1]: *** [generate_assets] Error 2
generated/simulator/gcc/Makefile:149: recipe for target 'generate_assets' failed
simulator/gcc/Makefile:32: recipe for target 'all' failed
make: *** [all] Error 2
Failed
I will be glad if someone could help me,
Thanks
Solved! Go to Solution.
2020-12-21 9:29 PM
Hello GC2,
A new version of TouchGFX is available (4.16). In this version, the getSelectedPage() is implemented. You can download it from this link : https://my.st.com/content/my_st_com/en/products/development-tools/software-development-tools/stm32-software-development-tools/stm32-configurators-and-code-generators/touchgfxdesigner.html
When your question is answered, please close this topic by choosing Select as Best.
/Alexandre
2020-12-21 9:29 PM
Hello GC2,
A new version of TouchGFX is available (4.16). In this version, the getSelectedPage() is implemented. You can download it from this link : https://my.st.com/content/my_st_com/en/products/development-tools/software-development-tools/stm32-software-development-tools/stm32-configurators-and-code-generators/touchgfxdesigner.html
When your question is answered, please close this topic by choosing Select as Best.
/Alexandre
2020-12-22 12:06 AM
Hi, thanks for the informations. I've just updated my touchGFX version and try to compile it....if I run target from the designer is ok, but if i try to build from the IDE I got this error:
arm-none-eabi-g++ -o "STM32H735G-DK.elf" @"objects.list" -l:libtouchgfx-float-abi-hard.a -mcpu=cortex-m7 -T"C:\.........\STM32H735IGKX_FLASH.ld" --specs=nosys.specs -Wl,-Map="STM32H735G-DK.map" -Wl,--gc-sections -static -LC:/........../Middlewares/ST/touchgfx/lib/core/cortex_m7/gcc -LC:/.........../Middlewares/ST/touchgfx/lib/core/cortex_m7/gcc -LC:/................../Middlewares/ST/touchgfx/lib/core/cortex_m7/gcc -LC:/.........../Middlewares/ST/touchgfx/lib/core/cortex_m7/gcc -LC:.........../Middlewares/ST/touchgfx/lib/core/cortex_m7/gcc -LC:/.............../Middlewares/ST/touchgfx/lib/core/cortex_m7/gcc -LC:/............./Middlewares/ST/touchgfx/lib/core/cortex_m7/gcc --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -Wl,--start-group -lc -lm -lstdc++ -lsupc++ -Wl,--end-group
Application/User/generated/Screen00ViewBase.o:(.rodata._ZTVN8touchgfx12MoveAnimatorINS_11AnalogClockEEE[_ZTVN8touchgfx12MoveAnimatorINS_11AnalogClockEEE]+0xcc): undefined reference to `touchgfx::AnalogClock::setAlpha(unsigned char)'
Application/User/generated/Screen00ViewBase.o:(.rodata._ZTVN8touchgfx12MoveAnimatorINS_11AnalogClockEEE[_ZTVN8touchgfx12MoveAnimatorINS_11AnalogClockEEE]+0xd0): undefined reference to `touchgfx::AnalogClock::getAlpha() const'
collect2.exe: error: ld returned 1 exit status
make: *** [makefile:77: STM32H735G-DK.elf] Error 1
"make -j8 all" terminated with exit code 2. Build might be incomplete.
08:48:31 Build Failed. 1 errors, 0 warnings. (took 19s.738ms)
I'm using:
touchGFX 4.16.0 (just updated)
CubeProgrammer 2.5.0
STM32CubeMx 6.1.0
STM32CubeIDE 1.4.0
2020-12-22 1:28 AM
Anyway, the getSelectedPage works! Thanks a lot.
I wait for the answer of the other problem and then I will close the topic by choosing Select as best!
2020-12-22 8:53 PM
Hello GC2,
It says setAlpha() and getAlpha() are undefined. These 2 functions were added to the AnalogClock in 4.16. In 4.15 they didn't exist.
You updated TouchGFX Designer to 4.16 but have you also updated TouchGFX Generator in CubeMX ? The version must be also 4.16 in CubeMX otherwise you will have incompatibilities.
/Alexandre
2020-12-22 11:44 PM
Hi,
yes I've already done it before the last message.
The steps I've done were:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.