2020-09-30 5:10 AM
Hi,
Consider the following two CustomContainers and the Screen class :
class CustomContainer : public touchgfx::Container
{
public:
CustomContainer()
{
add(_a_text_area);
}
void setup(); //a function to setup the element
void writeText(const std::u16string txt)
{
_a_text_area.setVisible(false);
_a_text_area.invalidate();
_txt_buffer = txt;
_a_text_area.setWildcard((uint16_t*)&_txt_buffer[0]);
_a_text_area.resizeToCurrentText();
_a_text_area.setVisible(true);
_a_text_area.invalidate();
}
private:
touchgfx::TextAreaWithOneWildcard _a_text_area;
std::u16string _txt_buffer;
};
class CustomContainerBis : public touchgfx::Container
{
public:
CustomContainerBis();
void setup(const uint8_t elements_nb)
{
//here, I've tried various other solutions to setup the vector
_custom_containers = std::vector<CustomContainer>(6, CustomContainer());
//place CustomContainer objects and set them up
int y = 0;
for (int i = 0; i < 6; i++)
{
_custom_containers[i].setup();
_custom_containers[i].setPosition(0, y, 50, 15);
add(_custom_containers[i]);
y += 20;
}
setWidth(15);
setHeight(y);
}
void fillInElements()
{
for (int i = 0; i < (int)_custom_containers.size(); i++)
{
_custom_containers[i].writeText(u"a_text");
}
}
private:
std::vector<CustomContainer> _custom_containers;
};
class Screen : public ScreenBase
{
public:
Screen()
{
_a_custom_container.setXY(20, 20);
_a_custom_container.setup(5);
add(_a_custom_container);
}
void aFunction()
{
_a_custom_container.fillInElements();
}
private:
CustomContainerBis _a_custom_container;
}In this code, the line _a_text_area.invalidate() within the function writeText() throws an error message (reference to unknown object). What is it I'm doing wrong? I suspect it has to do with the call to the add(_a_text_area) fuction which is inside the default constructor…
Any help is more than welcome ! I've been struggling with this for quite some time now and tried a lot of different things… Ofc I can make it work by creating a vector of pointers to CustomContainer but It's not something I wish to do.
Guillaume.
Ps : excuse if there are any mistakes that slipped in the code above, I wrote it all off the top of my head…
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.