2020-06-04 2:01 AM
Hello I have a problem with reading data on I2C. My code goes HardFault error after this( while (hi2c->XferCount > 0U);)
line. I'm reallt stuck in here. Does anyone have idea about that?
HAL_StatusTypeDef HAL_I2C_Mem_Read(I2C_HandleTypeDef *hi2c, uint16_t DevAddress, uint16_t MemAddress, uint16_t MemAddSize, uint8_t *pData, uint16_t Size, uint32_t Timeout)
{
uint32_t tickstart;
/* Check the parameters */
assert_param(IS_I2C_MEMADD_SIZE(MemAddSize));
if (hi2c->State == HAL_I2C_STATE_READY)
{
if ((pData == NULL) || (Size == 0U))
{
hi2c->ErrorCode = HAL_I2C_ERROR_INVALID_PARAM;
return HAL_ERROR;
}
/* Process Locked */
__HAL_LOCK(hi2c);
/* Init tickstart for timeout management*/
tickstart = HAL_GetTick();
if (I2C_WaitOnFlagUntilTimeout(hi2c, I2C_FLAG_BUSY, SET, I2C_TIMEOUT_BUSY, tickstart) != HAL_OK)
{
return HAL_ERROR;
}
hi2c->State = HAL_I2C_STATE_BUSY_RX;
hi2c->Mode = HAL_I2C_MODE_MEM;
hi2c->ErrorCode = HAL_I2C_ERROR_NONE;
/* Prepare transfer parameters */
hi2c->pBuffPtr = pData;
hi2c->XferCount = Size;
hi2c->XferISR = NULL;
/* Send Slave Address and Memory Address */
if (I2C_RequestMemoryRead(hi2c, DevAddress, MemAddress, MemAddSize, Timeout, tickstart) != HAL_OK)
{
/* Process Unlocked */
__HAL_UNLOCK(hi2c);
return HAL_ERROR;
}
/* Send Slave Address */
/* Set NBYTES to write and reload if hi2c->XferCount > MAX_NBYTE_SIZE and generate RESTART */
if (hi2c->XferCount > MAX_NBYTE_SIZE)
{
hi2c->XferSize = MAX_NBYTE_SIZE;
I2C_TransferConfig(hi2c, DevAddress, (uint8_t)hi2c->XferSize, I2C_RELOAD_MODE, I2C_GENERATE_START_READ);
}
else
{
hi2c->XferSize = hi2c->XferCount;
I2C_TransferConfig(hi2c, DevAddress, (uint8_t)hi2c->XferSize, I2C_AUTOEND_MODE, I2C_GENERATE_START_READ);
}
do
{
/* Wait until RXNE flag is set */
if (I2C_WaitOnFlagUntilTimeout(hi2c, I2C_FLAG_RXNE, RESET, Timeout, tickstart) != HAL_OK)
{
return HAL_ERROR;
}
/* Read data from RXDR */
*hi2c->pBuffPtr = (uint8_t)hi2c->Instance->RXDR;
/* Increment Buffer pointer */
hi2c->pBuffPtr++;
hi2c->XferSize--;
hi2c->XferCount--;
if ((hi2c->XferCount != 0U) && (hi2c->XferSize == 0U))
{
/* Wait until TCR flag is set */
if (I2C_WaitOnFlagUntilTimeout(hi2c, I2C_FLAG_TCR, RESET, Timeout, tickstart) != HAL_OK)
{
return HAL_ERROR;
}
if (hi2c->XferCount > MAX_NBYTE_SIZE)
{
hi2c->XferSize = MAX_NBYTE_SIZE;
I2C_TransferConfig(hi2c, DevAddress, (uint8_t) hi2c->XferSize, I2C_RELOAD_MODE, I2C_NO_STARTSTOP);
}
else
{
hi2c->XferSize = hi2c->XferCount;
I2C_TransferConfig(hi2c, DevAddress, (uint8_t)hi2c->XferSize, I2C_AUTOEND_MODE, I2C_NO_STARTSTOP);
}
}
}
while (hi2c->XferCount > 0U);//////////////////////////////////////////////////////////////
/* No need to Check TC flag, with AUTOEND mode the stop is automatically generated */
/* Wait until STOPF flag is reset */
if (I2C_WaitOnSTOPFlagUntilTimeout(hi2c, Timeout, tickstart) != HAL_OK)
{
return HAL_ERROR;
}
/* Clear STOP Flag */
__HAL_I2C_CLEAR_FLAG(hi2c, I2C_FLAG_STOPF);
/* Clear Configuration Register 2 */
I2C_RESET_CR2(hi2c);
hi2c->State = HAL_I2C_STATE_READY;
hi2c->Mode = HAL_I2C_MODE_NONE;
/* Process Unlocked */
__HAL_UNLOCK(hi2c);
return HAL_OK;
}
else
{
return HAL_BUSY;
}
}
2020-06-04 5:06 AM
Did you check registers for errors to see if there's a hint?
2020-06-04 5:09 AM
Hi Martin,
After I wrote this I solve this issue it was just my bad. Thanks for reply.
2020-06-04 5:12 AM
Consider posting your solution so that others may learn.
2020-06-04 5:17 AM
it was just a problem caused by incorrectly sending the Length value to the reading function. Program goes into hard fault error because the value that should be 4 is much higher.
2020-06-04 5:20 AM
Good news :)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.