2021-04-09 7:17 PM
looks like I need user begin and end sections
const uint16_t BITMAP_ICON_KEYBOARD_EVEN_ROW_ID = 0;
const uint16_t BITMAP_ICON_KEYBOARD_HIGHLIGHTED_ID = 1;
const uint16_t BITMAP_ICON_KEYBOARD_ODD_ROW_ID = 2;
const uint16_t BITMAP_KEYBOARD_BACKGROUND_ID = 3;
const uint16_t BITMAP_KEYBOARD_KEY_DELETE_HIGHLIGHTED_ID = 4;
const uint16_t BITMAP_KEYBOARD_KEY_HIGHLIGHTED_ID = 5;
const uint16_t BITMAP_KEYBOARD_KEY_NUM_HIGHLIGHTED_ID = 6;
const uint16_t BITMAP_KEYBOARD_KEY_SHIFT_HIGHLIGHTED_ID = 7;
const uint16_t BITMAP_KEYBOARD_SPACE_HIGHLIGHTED_ID = 8;
2021-04-12 1:06 AM
Hi,
This is expected as the modifications made in files under the /generated folder will be overwritten when generating code from TouchGFX Designer (so also when using the simulator or running on target options from Designer).
/Romain
2021-04-12 1:11 AM
What are you trying to do by the way ? This is an old generated file containing information on the bitmaps generated by the image converter. It gets deleted at every code generation.
/Romain
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.