cancel
Showing results for 
Search instead for 
Did you mean: 

I can't find pinout information regarding LCD_R6, LCD_R7, LCD_HSYNC, LCD_VSYNC for STM32L4RVI LQFP100 case

AShap.18
Associate
 
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Danish1
Lead III

What I tend to do is a search of the data sheet for the peripheral pin I want, and Table 15 shows me which GPIO it shares, and what pin (if any) it is bonded to.

If I look in the data sheet for STM32L4R5xx, STM32L4R7xx and STM32L4R9xx DS12023 Rev 4 in Table 15

on page 97/310, I can see which pin PD11 is connected to (for LQFP100 this is not connected) and that one of its alternate functions is LCD_R6. So you can't use LCD_R6 if you have the LQFP100 package.

Similarly, on page 98/310, I see that LCD_R7 is PD12, again unavailable in LQFP100.

And on page 115/310, LCD_HSYNC is PE0 and LCD_VSYNC is PE1. But neither of them is bonded out for the LQFP100 package.

That's just one of the compromises of a package with fewer pins.

If you've chosen LQFP100 due to board size limitations, you might consider a BGA package. But they tend to need more complicated pcbs.

Hope this helps,

Danish

AShap.18
Associate

Thanks Danish,

should be worth to mention this on Data sheet, I've started already with LQFP100.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.