2020-07-25 2:30 AM
Hi, I'm using touchgfx on STM3F746-Disco kit, and I'm having some trouble with internal RAM, it's too small for my application. So I'm trying to configure my project to use SDRAM instead of internal RAM. And I mean my variables get auto allocated on SDRAM, not by using a function to put it on SDRAM. I've found some post about changing the linker file (.ld). But I just can make it work. Can someone help me with a detail linker script file for SDRAM.
2020-08-24 7:31 AM
Hello,
The linker file being dependent on the IDE you are using, what is your IDE ?
You can look at the H750-DK Application Template available in TouchGFX Designer for reference.
Also, when you write a post related to TouchGFX, please add TouchGFX as the Topic, otherwise we might not see it.
/Alexandre
2020-08-24 7:08 PM
I'm using STM32CubeIDE
2020-08-25 4:29 AM
The F750-DK Application Template uses also external RAM to store the framebuffers. YOu will find the .ld file in STM32CubeIDE/ folder.
Here is one extract :
/* Memories definition */
MEMORY
{
ITCMRAM (xrw) : ORIGIN = 0x00000000, LENGTH = 16K
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 320K
SDRAM (xrw) : ORIGIN = 0xC0000000, LENGTH = 8M
FLASH (xrw) : ORIGIN = 0x90000000, LENGTH = 1M
ASSETS_FLASH (r) : ORIGIN = 0x90100000, LENGTH = 15M
BOOTLOADER (xrw) : ORIGIN = 0x08000000, LENGTH = 64k
}
/* ... */
BmpCacheSection (NOLOAD) : { *(BmpCacheSection) } >SDRAM
TouchGFX_Framebuffer (NOLOAD) : { *(TouchGFX_Framebuffer) } >SDRAM
TouchGFX_Framebuffer1 (NOLOAD) : { *(TouchGFX_Framebuffer1) } >SDRAM
TouchGFX_Framebuffer2 (NOLOAD) : { *(TouchGFX_Framebuffer2) } >SDRAM/Alexandre
2020-08-25 8:55 PM
Thanks to you, I've found that file, I'll follow that file
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.