2020-02-29 12:11 AM
2020-03-13 6:04 AM
Hello Martin,
There is no example available for FMC NOR flash used to store touchgfx assets in cube firmware examples/projects. Only i could find examples where QSPI flash is used for touchgfx.
I have done necessary initialization for FMC NOR flash and also described the Flash memory region in the linker script as follows, but it dint work. I am using stm32f769i eval board for the same. FMC nor flash is memory mapped. Also i have taken care the caching part using mpu config for nor flash and in sdram. kindly let me know where could be the issue.
LR_ROM1 0x60000000 0x01000000 { ; load region size_region
extflash.bin 0x60000000 0x01000000 { ; load address = execution address
*.o (ExtFlashSection)
}
}
2020-03-13 6:07 AM
What actually is your problem? Can you read from your NOR flash? What "didn't work" ?
/Martin
2020-03-13 6:20 AM
NOR flash works fine, i can independently read and write but when i am using it for touchgfx, the stored images are not getting displayed / retrieved. Also the frame buffer is resident on FMC sdram.
2020-03-13 7:04 AM
And your application is running fine, otherwise?
2020-03-13 7:22 AM
yes it does only not able to retrieve images from FMC NOR flash
2020-03-15 11:35 PM
so is it possible for you to experiment with FMC NOR flash to store touchgfx assets and share an example or can u plz let me knw what i can try as FMC NOR flash is memory mapped
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.