2020-07-09 6:14 AM
2020-07-09 6:55 AM
Hello,
You can refer to any Application Template available on TouchGFX Designer but for instance you can look at the Application Template STM32F746G-DISCO with the TouchGFX Demo 1. This will tell you how both on the hardware development and GUI development side you implement the MCU load.
/Alexandre
2020-07-17 4:55 AM
Here's a few extra pointers to look for in any of the demos that Alexandre mentioned.
This code is required in FreeRTOSConfig.h
/* USER CODE BEGIN Defines */
/* Section where parameter definitions can be added (for instance, to override default ones in FreeRTOS.h) */
#define traceTASK_SWITCHED_OUT() xTaskCallApplicationTaskHook( pxCurrentTCB, (void*)1 )
#define traceTASK_SWITCHED_IN() xTaskCallApplicationTaskHook( pxCurrentTCB, (void*)0 )
/* USER CODE END Defines */If you're using FreeRTOS - this code is required in your OSWrappers.cpp. We don't have examples for other OS.
// FreeRTOS specific handlers
extern "C"
{
void vApplicationStackOverflowHook(xTaskHandle xTask,
signed portCHAR* pcTaskName)
{
while (1);
}
void vApplicationMallocFailedHook(xTaskHandle xTask,
signed portCHAR* pcTaskName)
{
while (1);
}
void vApplicationIdleHook(void)
{
// Set task tag in order to have the "IdleTaskHook" function called when the idle task is
// switched in/out. Used solely for measuring MCU load, and can be removed if MCU load
// readout is not needed.
vTaskSetApplicationTaskTag(NULL, IdleTaskHook);
}
}Then some MCU Instrumentation is required in order to get the clocl cycle count for a particular MCU family, in this case F7 - TouchGFX HAL will call these functions if instrumentation is configured.
#include <bsp/STM32F7Instrumentation.hpp>
#include <touchgfx/hal/HAL.hpp>
extern "C"
{
#include "stm32756g_eval_sdram.h"
#include "stm32756g_eval_lcd.h"
#include "stm32756g_eval_io.h"
#include "stm32756g_eval_nor.h"
#include "stm32f7xx_hal_dma.h"
#include "stm32f7xx_hal_qspi.h"
#include "stm32f7xx_hal_rcc_ex.h"
#include "stm32f7xx_hal_tim.h"
}
namespace touchgfx
{
TIM_HandleTypeDef tim;
void STM32F7Instrumentation::init()
{
__TIM2_CLK_ENABLE();
tim.Instance = TIM2;
tim.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
tim.Init.CounterMode = TIM_COUNTERMODE_UP;
tim.Init.Period = 0xFFFFFFFF;
tim.Init.Prescaler = 0;
tim.Init.RepetitionCounter = 1;
HAL_TIM_Base_Init(&tim);
HAL_TIM_Base_Start(&tim);
}
//Board specific clockfrequency
unsigned int STM32F7Instrumentation::getElapsedUS(unsigned int start, unsigned int now, unsigned int clockfrequency)
{
return ((now - start) + (clockfrequency / 2)) / clockfrequency;
}
unsigned int STM32F7Instrumentation::getCPUCycles()
{
return __HAL_TIM_GET_COUNTER(&tim);
}
void STM32F7Instrumentation::setMCUActive(bool active)
{
if (active) //idle task sched out
{
cc_consumed += getCPUCycles() - cc_in;
}
else //idle task sched in
{
cc_in = getCPUCycles();
}
}
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.