2020-01-29 8:51 AM
My office computer only have internet access via virtual machine, So i can't download the templates in the TouchGFX Designer.
How to install the STM32F746G-DISCO template offline?
Solved! Go to Solution.
2020-01-30 1:10 AM
Place AT package files into app/packages of your designer install. e.g. for mine:
D:\TouchGFX\4.13.0\app\packagesYou will have to request them, for now, to get the files. Which ones do you need?
/Martin
2020-01-29 10:24 AM
USB memory stick?
2020-01-29 2:15 PM
My problem is were to download the template files and know in what directories the files should be transferred to.
2020-01-30 1:10 AM
Place AT package files into app/packages of your designer install. e.g. for mine:
D:\TouchGFX\4.13.0\app\packagesYou will have to request them, for now, to get the files. Which ones do you need?
/Martin
2020-01-30 3:48 AM
Martin,
I need the last template for the "STM32F746G Discovery Kit".
Another PC with the template installed, in the directory C:\TouchGFX\4.13.0\app\packages, it only have the files:
BlankUI-2.0.0.tpa
Simulator-2.0.0.tpa
2020-01-30 4:09 AM
The two templates that you're referring to are simply the two default packages that the designer comes installed with.
The actual packages you've downloaded are inside %APPDATA%/Touchgfx-4.13.0/Downloads
2020-01-30 4:09 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.