2022-03-23 10:46 PM
I want to verify that the STM32L4R9 discovery kit can work in DSI video mode so that I can port the application to use a display driver that does not have a graphics buffer. I started with the TouchGFXWatch example and have that working. I then used TouchGFX Generator to change the Display Interface to Parallel RCB (LTDC) (per advice from the forum). This resulted in the initial display but no update. I then changed DSIHost to Video Mode which resulted in stripy noise being displayed. I believe I am using the latest versions of all the tools: TouchGFX 4.19, CubeMX 6.5.0, STM32CubeIDE 1.8.0.
My forum reading suggests that this is hard, but possible. Can anyone enlighten me on what I need to modify under the hood to get this to work?
2022-04-22 11:13 PM
2022-04-23 12:11 AM
This is the generated code when I enable PSRAM via FMC:
static void MX_FMC_Init(void)
{
/* USER CODE BEGIN FMC_Init 0 */
/* USER CODE END FMC_Init 0 */
FMC_NORSRAM_TimingTypeDef Timing = {0};
/* USER CODE BEGIN FMC_Init 1 */
/* USER CODE END FMC_Init 1 */
/** Perform the SRAM1 memory initialization sequence
*/
hsram1.Instance = FMC_NORSRAM_DEVICE;
hsram1.Extended = FMC_NORSRAM_EXTENDED_DEVICE;
/* hsram1.Init */
hsram1.Init.NSBank = FMC_NORSRAM_BANK1;
hsram1.Init.DataAddressMux = FMC_DATA_ADDRESS_MUX_DISABLE;
hsram1.Init.MemoryType = FMC_MEMORY_TYPE_PSRAM;
hsram1.Init.MemoryDataWidth = FMC_NORSRAM_MEM_BUS_WIDTH_16;
hsram1.Init.BurstAccessMode = FMC_BURST_ACCESS_MODE_ENABLE;
hsram1.Init.WaitSignalPolarity = FMC_WAIT_SIGNAL_POLARITY_LOW;
hsram1.Init.WaitSignalActive = FMC_WAIT_TIMING_BEFORE_WS;
hsram1.Init.WriteOperation = FMC_WRITE_OPERATION_ENABLE;
hsram1.Init.WaitSignal = FMC_WAIT_SIGNAL_DISABLE;
hsram1.Init.ExtendedMode = FMC_EXTENDED_MODE_DISABLE;
hsram1.Init.AsynchronousWait = FMC_ASYNCHRONOUS_WAIT_DISABLE;
hsram1.Init.WriteBurst = FMC_WRITE_BURST_ENABLE;
hsram1.Init.ContinuousClock = FMC_CONTINUOUS_CLOCK_SYNC_ONLY;
hsram1.Init.WriteFifo = FMC_WRITE_FIFO_ENABLE;
hsram1.Init.NBLSetupTime = 0;
hsram1.Init.PageSize = FMC_PAGE_SIZE_NONE;
/* Timing */
Timing.AddressSetupTime = 15;
Timing.AddressHoldTime = 15;
Timing.DataSetupTime = 255;
Timing.DataHoldTime = 0;
Timing.BusTurnAroundDuration = 15;
Timing.CLKDivision = 2;
Timing.DataLatency = 2;
Timing.AccessMode = FMC_ACCESS_MODE_A;
/* ExtTiming */
if (HAL_SRAM_Init(&hsram1, &Timing, NULL) != HAL_OK)
{
Error_Handler( );
}
/* USER CODE BEGIN FMC_Init 2 */
/* USER CODE END FMC_Init 2 */
}And this is the display when I set the GFXMMU to point to the external ram - I'm pretty sure that the image is there, buried in the noise
2022-04-23 2:04 AM
Things have substantially improved - I found settings from a HAL file for the board and the display is almost there. FMC settings:
hsram1.Init.NSBank = FMC_NORSRAM_BANK1;
hsram1.Init.DataAddressMux = FMC_DATA_ADDRESS_MUX_DISABLE;
hsram1.Init.MemoryType = FMC_MEMORY_TYPE_PSRAM;
hsram1.Init.MemoryDataWidth = FMC_NORSRAM_MEM_BUS_WIDTH_16;
hsram1.Init.BurstAccessMode = FMC_BURST_ACCESS_MODE_DISABLE;
hsram1.Init.WaitSignalPolarity = FMC_WAIT_SIGNAL_POLARITY_HIGH;
hsram1.Init.WaitSignalActive = FMC_WAIT_TIMING_BEFORE_WS;
hsram1.Init.WriteOperation = FMC_WRITE_OPERATION_ENABLE;
hsram1.Init.WaitSignal = FMC_WAIT_SIGNAL_DISABLE;
hsram1.Init.ExtendedMode = FMC_EXTENDED_MODE_DISABLE;
hsram1.Init.AsynchronousWait = FMC_ASYNCHRONOUS_WAIT_DISABLE;
hsram1.Init.WriteBurst = FMC_WRITE_BURST_DISABLE;
hsram1.Init.ContinuousClock = FMC_CONTINUOUS_CLOCK_SYNC_ASYNC;
hsram1.Init.WriteFifo = FMC_WRITE_FIFO_DISABLE;
hsram1.Init.NBLSetupTime = 0;
hsram1.Init.PageSize = FMC_PAGE_SIZE_NONE;Timings:
Timing.AddressSetupTime = 1;
Timing.AddressHoldTime = 0;
Timing.DataSetupTime = 5;
Timing.BusTurnAroundDuration = 1;
Timing.CLKDivision = 2;
Timing.DataLatency = 2;
Timing.AccessMode = FMC_ACCESS_MODE_A;But I don't think they match the device timings (attached). I've experimented with many values and what I have is close to working but not quite there. Can anyone with a better understanding of PSRAM timings advise?
2022-04-23 4:44 AM
Hi Olync,
I'm not an expert on PSRAM but digging around, there does look to be an example FMC project for your disco on the ST repository.
The example uses the following timing:
SRAM_Timing.AddressSetupTime = 5;
SRAM_Timing.AddressHoldTime = 1; /* Min value, Don't care on SRAM Access mode A */
SRAM_Timing.DataSetupTime = 3;
SRAM_Timing.BusTurnAroundDuration = 1;
SRAM_Timing.CLKDivision = 2; /* Min value, Don't care on SRAM Access mode A */
SRAM_Timing.DataLatency = 2; /* Min value, Don't care on SRAM Access mode A */The clock is the example is configured at 80MHz or (12.5ns period) so these settings seem reasonable compared to datasheet specifications.
Cheers.
2022-04-24 12:57 AM
Thanks all for your help, I finally got it working with double buffering in PSRAM. The last hurdle was annoying full screen glitches periodically. I tracked it down to this framework-generated code:
void TouchGFXHAL::setTFTFrameBuffer(uint16_t* adr)
{
if (doubleBufferingEnabled)
{
HAL_DSI_Stop(&hdsi);
currFbBase = adr;
/* Update LTDC layers base address */
if (HAL_LTDC_SetAddress(&hltdc, (uint32_t)currFbBase, 0) != HAL_OK)
{
while (1);
}
__HAL_LTDC_LAYER_ENABLE(&hltdc, 0);
__HAL_LTDC_RELOAD_IMMEDIATE_CONFIG(&hltdc);
HAL_DSI_Start(&hdsi);
}
}I commented out the HAL_DSI_Stop and HAL_DSI_Start - hey presto, no flicker! Not sure how legit it is but it's working!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.