2021-03-02 8:36 PM
The interface of the stm32f469i_Discovery LCD is MIPI.
It wants to replace LCDs with other MIPI interfaces.
The control IC of the LCD I want to use uses the ILI9806E.
I inquired about LCD supplier, and they said that LCD initialization code is initialized inside LCD module, so there is nothing to do, but just need to adjust MIPI interface.
I want to modify the stm32F469I_Discovery LCD code and match it with the ILI9806E, but I don't need the LCD initialization code, so can you tell me how to set the MIPI interface?
What I think is that you just need to delete the LCD initialization code from the existing code and adjust the data related to the resolution, should I do other things?
Solved! Go to Solution.
2021-03-03 4:57 AM
Yes, hollowing out an existing driver and then constructing a new implementation is a workable approach.
You might also want to look at the F7 libraries and examples, especially the F769-DISCO, which had the detachable screen, and with HDMI and RPI adapters.
Certainly possible to adapt the HDMI one to timings for 800x480 and 1024x600 type displays.
2021-03-03 4:57 AM
Yes, hollowing out an existing driver and then constructing a new implementation is a workable approach.
You might also want to look at the F7 libraries and examples, especially the F769-DISCO, which had the detachable screen, and with HDMI and RPI adapters.
Certainly possible to adapt the HDMI one to timings for 800x480 and 1024x600 type displays.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.