2018-12-12 8:33 AM
I have a STM32F0-DISCOVERY board that I've connected a sampling capacitor and a single touch button to. I've generated code in CubeMX for this configuration and have all the coed in my TrueStudio project. I want to use STM Studio to tune my touch button settings. What are the functions I need to add to my code (assuming the only thing my code does is run this touch button) to initialize and run the button?
CubeMX adds:
HAL_Init()
SystemClock_Config()
MX_GPIO_Init()
MX_TSC_Init()
MX_TOUCHSENSING_Init()
I have added TSL_tkey_Init() before the while(1) loop. Inside the while loop I have tsl_user_Exec() and TSL_tkey_Process().
When I run the program, Ref and RefRest stay at 0, StateId stays at 0 (calibration), but the Delta is about -600 and reacts to touches. What steps am I missing?
2018-12-12 1:24 PM
I think I figured it out: my sample capacitor was not soldered on very well.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.