2023-09-12 5:35 AM
Hi ,
I've implemented multiple screen in my project(Custom project using STM32F429zi controller with external RAM and Flash). I'm getting memory fault issue whenever I'm transitioning from one particular screen to any other screen. When I debugged I got source of problem at below mentioned line
assert(sizeof(TransType) <= heap.transitionStorage.element_size() && "Transition allocation error: Check that all transitions are added to FrontendHeap::TransitionTypes");
in function
'PresenterType* makeTransition(Screen** currentScreen, Presenter** currentPresenter, MVPHeap& heap, Transition** currentTrans, ModelType* model)'
under file 'mvp/MVPApplication.hpp'
I think I've added more widget and container to screen, due to which during transitioning it is crossing allocated heap memory for transitioning screen, correct me if I'm wrong here. If yes , how can we increase allocated heap for screen transition.
thank you.
2023-09-13 9:22 PM
Hi
There is a file called FrontendHeap.hpp
There you have to add your user-defined ViewTypes, PresenterTypes and TransitionTypes
typedef touchgfx::meta::TypeList< touchgfx::meta::Nil, //Replace this with first user-defined type
touchgfx::meta::Nil //List must always end with meta::Nil !
> UserDefinedViewTypes;
/* List any user-defined presenter types here*/
typedef touchgfx::meta::TypeList< touchgfx::meta::Nil, //Replace this with first user-defined type
touchgfx::meta::Nil //List must always end with meta::Nil !
> UserDefinedPresenterTypes;
/* List any user-defined transition types here*/
typedef touchgfx::meta::TypeList< touchgfx::meta::Nil, //Replace this with first user-defined type
touchgfx::meta::Nil //List must always end with meta::Nil !
> UserDefinedTransitionTypes;
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.