2020-11-06 12:42 PM
Generator create this part not exist in touchgfx project file. But is fine have it here for direct compile and flash. Why this isnt used? Howto add make ... flash here manualy?
Solved! Go to Solution.
2020-12-19 10:49 AM
@Alexandre RENOUX i save your time, solution for my problem is change Compile Target command to :
cd c:\ST\STM32CubeIDE_1.1.0\STM32CubeIDE\ && headless-build.bat -project Ex_ST_DSI/Debug -workspace C:\Users\Public\CubeWorkspace -build -console
++folders need be changed to user installed places,
but installed CubeIDE is required. I still see idea to TouchGFX implement functional compile and flash, hope developers do it.
2020-11-09 7:38 PM
Hello,
2 solutions :
Simply create an Application Template from TouchGFX and copy paste this section. All Application templates have this correctly set and it does not change depending on the board/project.
When your question is answered, please close this topic by choosing Select as Best.
/Alexandre
2020-11-10 8:11 AM
Hmm Alexandra i ask howto not where, i ofcourse know where i can write commands, but IDE makefile i mean isnt able use flash ...
Your reply is unusable
2020-11-21 1:51 AM
I solve this with enter to
Compile target command : cd ../Debug && make all -j8
and flash target command i create external cmd file, because write /\ here is little complicated , use any flash cli utility to load hex
place file to same directory as .touchgfx and enter name to
Flash Target Command : flashit.cmd
Thats all.
2020-12-15 8:10 AM
I test it more , but work only when no files is added to project. Then here we need better solution.
Now only flash over IDE work.
2020-12-15 5:40 PM
Hello MM..1,
If you are talking about the fact that you cannot "Run Target" from TouchGFX Designer when creating your own project from CubeMX. This is normal and my previous answer should solve your problem.
If you are talking about something else, sorry please elaborate because unfortunately, I still don't understand your point.
/Alexandre
2020-12-16 7:55 AM
No i talk about Compile target command : cd ../Debug && make all -j8
My project is created in IDE as new from zero. Then choice MCU and in MX plugin configure all plus touchgfx.
Then Touchgfx have Target parts empty, but editable. And i need for graphic designer create environment withour IDE use for flash and run target on real hardware. All this now work with up command, but when designer add font or image or anything, that generates new cpp files, then make all get error, because in debug subdirs mk files isnt updated by TouchGFX. Now i hope you understand.
2020-12-17 12:54 AM
Why do you not want to use the makefile in /gcc folder ? There's nothing related to CubeIDE inside. It uses gcc to compile that is all.
Your intention and why you think the current Run Target option is a problem, is blurry to me.
If you are talking about flashing, when using external memories, you need to use CubeProgrammer with external loader to flash the assets (texts, images, ...) in external memory.
You talk about ../Debug but what is the complete path of this folder ?
make should work if you are in the correct folder including the makefile.
If you actually use the correct makefile and you have these errors, please specify the exact steps you did. Enclosing the makefile to your answer can also help.
/Alexandre
2020-12-17 8:02 AM
Directory of c:\TouchGFXProjects\Testroj_TouchGFX
19.11.2020 20:04 <DIR> .
19.11.2020 20:04 <DIR> ..
19.11.2020 20:09 43 435 .cproject
19.11.2020 20:04 19 871 .mxproject
19.11.2020 19:56 1 358 .project
16.12.2020 17:58 <DIR> .settings
10.11.2020 13:02 <DIR> Core
19.11.2020 20:08 <DIR> Debug
10.11.2020 13:02 <DIR> Drivers
10.11.2020 13:02 <DIR> Middlewares
19.11.2020 20:04 26 371 Nu-MENU_TouchGFX.ioc
28.10.2020 08:49 7 524 Testproj_TouchGFX Debug.launch
19.11.2020 20:04 4 671 STM32F429ZITX_FLASH.ld
06.07.2020 11:21 4 671 STM32F429ZITX_FLASH.ld.boot
28.10.2020 09:51 4 671 STM32F429ZITX_FLASH.ld.orig
27.10.2020 11:22 4 637 STM32F429ZITX_RAM.ld
19.11.2020 20:04 <DIR> TouchGFXThis is unsorted dirlist for standart CubeIDE created project, and here exist only 3 files named makefile. Two is in simulator dirs and one in Debug.
Alexandre really try to do , what i wrote . Your gcc is simulator for windows and real project on hardware is my thread.
I repeat for you how to replicate my error:
2020-12-17 5:56 PM
As mentioned in my previous answer, please enclose the makefile you are using. Even your entire project if not too big.
This is the easiest way.
/Alexandre
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.