2023-02-22 7:18 AM
hello, I try to get one when something not desired is detected by the camera and else 0 so I can use my custom trained CNN with the help of x cube ai.
Fp ai vision is used to display iamge on LCD how can I get my request by changing or adding the codes in it. I tried to add some code depending on the fp ai vision but it didn't work
2023-02-22 10:58 AM
/**
* @brief Get the subsequent frame available and:
* 1. send it to LCD for display
* 2. make it available for subsequent processing
* @param App_Context_Ptr pointer to application context
*/
void APP_GetNextReadyFrame(AppContext_TypeDef *App_Context_Ptr)
{
ValidationContext_TypeDef* Validation_Ctx_Ptr=&App_Context_Ptr->Test_ContextPtr->ValidationContext;
uint8_t* cam_capture_buff = App_Context_Ptr->Camera_ContextPtr->camera_capture_buffer;
#if MEMORY_SCHEME != FULL_INTERNAL_MEM_OPT
uint8_t* cam_frame_buff = App_Context_Ptr->Camera_ContextPtr->camera_frame_buffer;
#endif
if((App_Context_Ptr->Operating_Mode == VALID) && (Validation_Ctx_Ptr->validation_completed ==0))
{
TEST_GetNextValidationInput(App_Context_Ptr->Test_ContextPtr,
cam_capture_buff);
}
else if((App_Context_Ptr->Operating_Mode == DUMP) &&
(App_Context_Ptr->Test_ContextPtr->DumpContext.Dump_FrameSource == SDCARD_FILE))
{
TEST_GetNextDumpInput(App_Context_Ptr->Test_ContextPtr,
cam_capture_buff);
}
else
{
/* Wait for current camera acquisition to complete*/
while(App_Context_Ptr->Camera_ContextPtr->new_frame_ready == 0);
}
#if MEMORY_SCHEME != FULL_INTERNAL_MEM_OPT
if(App_Context_Ptr->Operating_Mode != VALID)
{
/****Coherency purpose: invalidate the camera_capture_buffer area in L1 D-Cache before CPU reading****/
UTILS_DCache_Coherency_Maintenance((void*)cam_capture_buff,
CAM_FRAME_BUFFER_SIZE, INVALIDATE);
}
/****Copy the camera_capture_buff buffer content onto the camera_frame_buff buffer so to release the camera capture buffer before triggering the subsequent camera frame capture****/
for(uint32_t i=0;i<CAM_RES_WIDTH*CAM_RES_HEIGHT*RGB_565_BPP; i++)
{
*((uint8_t *)(cam_frame_buff + i)) = *((uint8_t *)(cam_capture_buff + i));
}
#endif
}
ı think there should be a change in 1. send it to LCD for display part
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.