2020-10-26 8:21 AM
Hi everyone.
I have built many screens, and in every screen I have many single data and array data.
About single data I can transfer them to other screen, by save them to model when I close screen.
But I don't know how to save Array data (like Time [10]) to model when I close screen and get them when I active scree.
So Anyone can give me some advice to solve my problem
Thanks and best regards.
2020-10-26 6:34 PM
Hello,
Please have a look at the following article on our documentation website : https://support.touchgfx.com/docs/tutorials/tutorial-03
This should help you.
/Alexandre
2020-10-26 7:53 PM
Hi Alexandre RENOUX.
I have read Tutorial-03,and can transfer data to another screen via model, but it only single data like uint_8, uint_16.
Everything I need, that is I can transfer Array data to another screens line Time[10], Date[30].
Because if I using single data, it very long and must using many single data.
So can you help me in this case.
Thanks and best regards.
2020-10-26 9:32 PM
I see that you are not familiar with c and c++ programming. In these languages, you have something called pointers.
https://www.tutorialspoint.com/cplusplus/cpp_passing_arrays_to_functions.htm
/Alexandre
2020-10-26 11:32 PM
Yes, You right, I'm not familiar with c and c++ programming, thanks for your share.
But I don't know how to declare Array in the model.ccp like:
Model::Model() : modelListener(0), hour(0), minute(0)
{
}
in my know, hour(0) and minute(0) is single variable, but now I need declare Array in this that.
I tried to declared as bellow:
Model::Model() : modelListener(0), Array1[10],*Array2
{
}
But is don't correct.
Can you show me, how to declare Array in this case.
Thanks you so much.
2020-10-29 9:57 PM
Simply write in Model.hpp
int array1[10];I don't know if you are trying to use int or not but just put whatever type you need.
This forum is not meant to teach people how to code in c or c++. Please look on the internet for how to declare arrays, what's a a class, a constructor, ...etc
/Alexandre
2020-10-29 11:13 PM
Hi.
Maybe you don't read my question carefully.
I asked that how to declare Array in the model.ccp like some single variable like:
Model::Model() : modelListener(0), hour(0), minute(0)
{
}
Absolutely before that I must declared in model.hpp:
int array1[10];
In my know, hour(0) and minute(0) make initiate value for hour and minute variable, but now I need declare Array in this that.
I tried to declared as bellow:
Model::Model() : modelListener(0), Array1[10],*Array2
{
}
But is don't correct.
2020-11-01 10:32 PM
My bad.
If you want to initiate the values, simply do it inside the brackets
Model::Model() : modelListener(0)
{
// Do it here but here is an example
for(int i = 0; i < 10; i++)
{
array1[i] = 0;
}
}/Alexandre
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.