2021-03-08 4:11 AM
I define two different buttons. Pressing the first button activates the second button, and when the second button is pressed, the first button becomes active. can you help me thank you very much
2021-03-08 4:56 AM
Hi,
Thank you for reporting this, I just tested as well on my side and the touch does not work on that revision (works for older ones). I have warned the team to fix this.
/Romain
2021-03-08 5:01 AM
Thank you. Is the problem software or hardware? When will it be fixed?
yes old version pcb also works.
2021-03-09 1:22 AM
Hi,
It needs investigation but by looking at the data sheet for the two revisions and the user manual found here it seems like a hardware change: "SF-TC240T-9370-T replaced by FRD240C48003-B". They have changed the display between the revision C which works and the E revision.
I do not have a date for when it will be fixed but this does not seem to be too complicated. You can probably do the fixes yourself in CubeMX if you cannot wait for the updated application template by looking at the documentation and the datasheet of the E revision.
/Romain
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.