2023-06-26 2:19 PM
Hey all, experienced developer but new to ST ecosystem.
I have a STM32H7B3I-EVAL board and made my first project using TouchGFX Designer 4.21.4. I put on a Dynamic Graph and a few Text Areas with wildcards, and coded up some random data to try it out. Sporadically, I'd see the UI hang. I was able to catch it with a debugger and found it deadlocked with this stacktrace:
Thread #2 [TouchGFXTask] 604023232 (RUNNING) (Suspended : Breakpoint)
touchgfx::OSWrappers::takeFrameBufferSemaphore() at OSWrappers.cpp:72 0x800186a
touchgfx::HAL::lockFrameBuffer() at 0x8010c06
touchgfx::HAL::lockFrameBufferForRenderingMethod() at 0x8010c3a
touchgfx::Canvas::render() at 0x8024c82
touchgfx::GraphElementLine::drawCanvasWidget(touchgfx::Rect const&) const at 0x8012116
touchgfx::CanvasWidget::draw(touchgfx::Rect const&) const at 0x8010f44
touchgfx::Screen::JSMOC() at 0x8017540
touchgfx::Screen::startSMOC() at 0x8017596
touchgfx::Screen::draw() at 0x80175c4
touchgfx::Application::draw() at 0x8015ab4
touchgfx::Application::drawCachedAreas() at 0x8016948
touchgfx::HAL::tick() at 0x8010266
TouchGFXHAL::taskEntry() at TouchGFXHAL.cpp:68 0x8001682
touchgfx_taskEntry() at TouchGFXConfiguration.cpp:72 0x8001f2e
TouchGFX_Task() at app_touchgfx.c:89 0x8001366
I have no custom code that deals with the framebuffer; just stock widgets as mentioned. I attempted to find who was holding the semaphore, and found it was *maybe* _ZN8touchgfx13DMA_Interface10addToQueueERKNS_6BlitOpE, but can't help any further because that's in closed code with no debug info.
The hang is very irregular. Sometimes it would happen after nearly every reboot within 10 seconds. Sometimes I've gone for weeks with nothing. Once it took a whole weekend to hit. The following is speculation since it happens so rarely: It might happen more if the DynamicGraph rescales and does a slow invalidate of the entire graph. Having an opaque Box behind the graph seemed to make it happen less often. I have turned off DMA2D and have not seen it hang lately but don't have enough run time to confidently say it's related.
I've since moved on in this project and sorry that I don't have any minimal reproducible code to share. I thought I'd throw this stack trace out there to see if anybody else has seen it. I'm also investigating a custom OSWrappers workaround to detect and recover the hung UI task without affecting other FreeRTOS tasks.
2023-06-28 5:22 AM
Try increasing the TouchGFX task stack size. I had a similar problem when it was 1024 bytes. I am currently at 2048 and everything is ok.
Regards, Bobby
2023-06-28 8:08 AM
Thanks for the reply. I am at the project defaults for this board and it looks like the task has 4096 words of stack; I can't imagine why that's not enough.
const osThreadAttr_t TouchGFXTask_attributes = {
.name = "TouchGFXTask",
.stack_size = 4096 * 4,
.priority = (osPriority_t) osPriorityNormal,
};
2023-06-28 8:58 AM
It's more than enough. Apparently it's not that
2023-07-12 2:09 PM
Hello @Mark999 ,
There has been a case created to resolve this question and we will be reaching out to you directly.
Regards,
Roger
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.