2025-02-20 1:43 AM - edited 2025-02-20 1:46 AM
Dear Gfx Team,
When opening a project from 'My Recent Projects', could it behave as when [File > Open] i.e. opening it in current instance of the Designer.
If user wants a new Desiner, that could be done with Ctrl+click
Thank you
Solved! Go to Solution.
2025-02-27 6:16 AM
Hello @ferro ,
We will implement this feature in a future major release.
Regards,
2025-02-20 5:43 AM
Hello @ferro ,
Thank you for sharing your feedback.
I will discuss this matter with the team. However, for recent projects, we have intentionally opted to open a new instance of TouchGFX Designer. Therefore, I anticipate that there will be no changes to this approach.
Could you please outline the advantages of replacing the current project with the new one rather than opening a new instance of TouchGFX Designer?
Regards,
2025-02-20 6:54 AM - edited 2025-02-20 6:55 AM
"Could you please outline the advantages of replacing the current project with the new one rather than opening a new instance of TouchGFX Designer?"
Certainly.
I do not need new Designer instance. With behaviour as it is, I then have to close the current/old Designer instance.
And dont want to search for new project with [File > Open] either - rather tiring.
What about instead of changing current behaviour (new instance), add Ctrl+click to replace current project.touchgfx. Win-Win.
2025-02-27 6:16 AM
Hello @ferro ,
We will implement this feature in a future major release.
Regards,
2025-04-02 2:34 AM
I just discovered that I can close current project with Ctrl+Q and then open new one from the 'Recent' list within current Designer instance. It seems this does what I wanted.
I think you can bin my request if you haven't already done so.
Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.