2020-08-11 8:45 AM
Migrated working project from Cube5.4 to 5.6 stop working.
After correcting all issues and compile without errors i debug code. Main have default GUItask and next two tasks added. Started code init all hw and start rtos, but display show nothing . I make test add after init grey level to framebuffer and it show ok. Too pattern generator show color horizontal and vertical ok.
When i debug two added task work ok.
Only GUI noting init ...
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_DMA_Init();
MX_SPI2_Init();
MX_I2C3_Init();
MX_ADC1_Init();
MX_CRC_Init();
MX_TIM2_Init();
/* USER CODE BEGIN 2 */
HAL_GPIO_WritePin(SPI_CS_GPIO_Port, SPI_CS_Pin, GPIO_PIN_RESET);
HAL_SPI_Transmit(&hspi2, (uint8_t *)"\0", 1, 5); //relay off
SPI_CS_GPIO_Port->BSRR = SPI_CS_Pin;
RC5_Init();
Turn_ON();
// EE_Write();
HAL_TIM_PWM_Start(&htim2,TIM_CHANNEL_1);//LCD_LIGHT
HAL_Delay(321);
/* USER CODE END 2 */
/* USER CODE BEGIN RTOS_MUTEX */
/* add mutexes, ... */
MX_FMC_Init();
memset((void *)disp_mem,0,6*1024*1024);
MX_DMA2D_Init();
MX_LTDC_Init();
MX_TIM1_Init();
MM_MX_DSI();
MX_TouchGFX_Init();
/* USER CODE END RTOS_MUTEX */
/* USER CODE BEGIN RTOS_SEMAPHORES */
/* add semaphores, ... */
/* USER CODE END RTOS_SEMAPHORES */
/* USER CODE BEGIN RTOS_TIMERS */
/* start timers, add new ones, ... */
/* USER CODE END RTOS_TIMERS */
/* USER CODE BEGIN RTOS_QUEUES */
/* add queues, ... */
/* USER CODE END RTOS_QUEUES */
/* Create the thread(s) */
/* definition and creation of defaultTask */
osThreadDef(defaultTask, StartDefaultTask, osPriorityNormal, 0, 4096);
defaultTaskHandle = osThreadCreate(osThread(defaultTask), NULL);
/* USER CODE BEGIN RTOS_THREADS */
/* add threads, ... */
//display test
TIM2->CCR1 = 0x1666;
HAL_DSI_PatternGeneratorStart(&hdsi, 0, 0);
HAL_Delay(1621);
HAL_DSI_PatternGeneratorStart(&hdsi, 0, 1);
HAL_Delay(321);
while (HAL_GPIO_ReadPin(SW_PWR_GPIO_Port, SW_PWR_Pin) == GPIO_PIN_SET);
HAL_DSI_PatternGeneratorStop(&hdsi);
HAL_Delay(321);
Encoder_Init();
//led pcb test potom inde TCA6424 ext
//SPI latch ULN test
//SPI_CS_GPIO_Port->BRR = SPI_CS_Pin;
HAL_GPIO_WritePin(SPI_CS_GPIO_Port, SPI_CS_Pin, GPIO_PIN_RESET);
HAL_SPI_Transmit(&hspi2, (uint8_t *)"\000", 1, 5); //relays
SPI_CS_GPIO_Port->BSRR = SPI_CS_Pin;
HAL_Delay(321); //stab ADC inputs without inputs and with unmute fix
HAL_ADC_Start_DMA(&hadc1, (uint32_t*)adc_buf, ADC_BUF_LEN);
HAL_Delay(100);
Preamp_Set_Input();
xTaskCreate(db_task, "DBTask",
512,
NULL,
osPriorityNormal,
NULL);
xTaskCreate(test_task, "LEDFadeTask",
512,
NULL,
osPriorityBelowNormal,
//osPriorityNormal,
NULL);
/* USER CODE END RTOS_THREADS */
/* Start scheduler */
osKernelStart();
/* We should never get here as control is now taken by the scheduler */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
void StartDefaultTask(void const * argument)
{
/* USER CODE BEGIN 5 */
MX_TouchGFX_Process();
/* Infinite loop */
for(;;)
{
osDelay(1);
}
/* USER CODE END 5 */
}
Solved! Go to Solution.
2020-08-25 10:58 AM
We try optimize code better in new version. We have custom board and LCD and need go to max possibble refresh rate.
Now dotclock LTDC 20MHz and DSI 60MHzx8
Display 480x1280 around 29,3Hz refresh, we try find way to go up, but sdram IS42S16400J is only 16bit ...
EDIT 1: Today i read one docu about FMC SPI displays and touchgfx and see, that custom display settings is for this purposes and not for my DSI display in video mode. Here need be set LTDC in CubeMX 5.6 and up and not custom.
EDIT 2: Code from CubeMX 5.6 now can use dot clock 30MHz and display refresh around 50Hz
2020-08-20 1:07 AM
Hello,
Have you tried comparing the new code with the old one ? There must be some differences.
/Alexandre
2020-08-24 10:18 AM
Of course Alexandra, must differ. First diff is main in Core\Src\ cube 5.4 have cpp , but 5.6 c file.
Second is TouchGFX\target\ dir
5.4:
HW_Init.hpp
STM32F4Instrumentation.cpp
STM32F4Instrumentation.hpp
STM32F4TouchController.hpp
STM32F4TouchController.cpp
STM32F4HAL.hpp
STM32F4HAL.cpp
STM32F4DMA.hpp
STM32F4DMA.cpp
touchgfx_gpio.cpp
BoardConfiguration.cpp
HW_Init.cpp
5.6
generated\
TouchGFXGPIO.cpp
STM32TouchController.cpp
STM32TouchController.hpp
TouchGFXHAL.cpp
TouchGFXHAL.hpp
and in generated
OSWrappers.cpp
STM32DMA.cpp
STM32DMA.hpp
TouchGFXGeneratedHAL.cpp
TouchGFXGeneratedHAL.hpp
TouchGFXConfiguration.cpp
Then some files in 5.6 is new some dont exist ...
I compare all and migrate from 5.4 some functions step by step , but 5.6 touchcode not work for me. No error.
On 5.4 i mean all thinks is started in hw_init.cpp and Boardconfig.cpp and all works.
On 5.6 where is same points nobody know.
2020-08-25 3:30 AM
Hello,
Yes migrating from 5.4 to 5.6 can involve quite a lot of changes and struggle.
Do you have to update your project because you need something not available in 5.4 ?
What board are you working on ? If you need to update to 5.6, I can suggest you to start a new project with the corresponding Application Template and do the porting of your code from your current project to the Application Template.
Note that 6.0 is out so porting to CubeMX 6.0 directly can be an option as well.
/Alexandre
2020-08-25 10:58 AM
We try optimize code better in new version. We have custom board and LCD and need go to max possibble refresh rate.
Now dotclock LTDC 20MHz and DSI 60MHzx8
Display 480x1280 around 29,3Hz refresh, we try find way to go up, but sdram IS42S16400J is only 16bit ...
EDIT 1: Today i read one docu about FMC SPI displays and touchgfx and see, that custom display settings is for this purposes and not for my DSI display in video mode. Here need be set LTDC in CubeMX 5.6 and up and not custom.
EDIT 2: Code from CubeMX 5.6 now can use dot clock 30MHz and display refresh around 50Hz
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.