2020-04-01 1:54 AM
Hi Martin,
I develop one application with touchGFX 4.13 and Keil for dedicated board based F429 (like EvalBoard).
Sometime, it 's seem that when I modify (suppress one text area or change the name ID etc..) my design screen with TouchGFX, I press "Generate Code" button, the status bar display "done" , but the generated code file.cpp is not updated. I don't know exactly when this update is not done ( on which criteria) ...
What I miss about this point?
Thks & rgds.
Philippe
2020-04-01 3:34 AM
That should never happen. I think you'll have to be more systematic in showing me this scenario, using screenshots, git, etc.
/Martin
2020-04-01 6:13 AM
2020-04-07 5:06 AM
is there anything in your designer log that indicates that files could not be updated because an outside program was locking them? This usually isn't a problem even with IDEs open.
2020-04-30 3:24 AM
Any updates from you on this?
2020-05-06 12:41 AM
Hi Martin , Not really update about this problem.. I work with it.... Workaround --> I close KEIL when I Generate the TouchGFX code :( .
And in you side, do you try it ?
Philippe
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.