2019-09-16 2:15 PM
I am just starting out with GFX and have a few questions if anyone has the time to help me out a bit.
6.Are there any additional widgets I can find somewhere ? Like meters and , scopes , waveform displays ?
7.If I do work on the code , can I open it , Run, Simulate in the gfx Designer or does all extra code only run on the STm?
8.Do I have to code to use mixins ?
9.Can I define a touch area , say I have a picture of a knob and I want it to react like a knob ?
I am sorry if this is all very obvious , just beginning , thanks for your time.
Yes, I am reading the knowledge base but is there a manual somewhere ?
Solved! Go to Solution.
2019-09-17 11:30 AM
Hi @LalalandAudio,
Briefly:
1) No
2) Yes. Use the designer to create the basic layout, interaction and animation configuration of your application. Then you'll write all your gui logic by hand in the specialized classes in gui/ (e.g. MyView will inherit from MyViewBase, generated by the designer). A scenario:
3) Check how the class is used in the screen definition code files (gui/) - Just copy the class definition source file and include it in your own specialized view
4) Yes you could do that with the box progress. But, yea, you won't get far without being able to write some code.
6) You only have the widgets available from the designer for now - Some things, like waveform displays, aren't widgets but more application specific things. You can do a waveform display using a Graph, and you'd have to do some coding to make it work the way you want.
7) You can run any application in the simulator - Press "run simulator" from the designer to run an application compiled with gcc. Or open the visual studio project in simulator/msvs. Let me know if you're having issues.
8) Some mixins are configurable from the designer (Like Draggable). They can be used manually in code as well.
9) Yes you can.
Don't apologize. I hope this answers your questions. I know some answers are brief, but i'd prefer if we dove into those individually if you say we should. The manual is more or less the knowledge based on touchgfx.zendesk.com, for now, until we can migrate to the ST documentation platform. You could check out the getting started tutorials, to get started.
https://touchgfx.zendesk.com/hc/en-us/categories/200529271
/Martin
2019-09-17 11:30 AM
Hi @LalalandAudio,
Briefly:
1) No
2) Yes. Use the designer to create the basic layout, interaction and animation configuration of your application. Then you'll write all your gui logic by hand in the specialized classes in gui/ (e.g. MyView will inherit from MyViewBase, generated by the designer). A scenario:
3) Check how the class is used in the screen definition code files (gui/) - Just copy the class definition source file and include it in your own specialized view
4) Yes you could do that with the box progress. But, yea, you won't get far without being able to write some code.
6) You only have the widgets available from the designer for now - Some things, like waveform displays, aren't widgets but more application specific things. You can do a waveform display using a Graph, and you'd have to do some coding to make it work the way you want.
7) You can run any application in the simulator - Press "run simulator" from the designer to run an application compiled with gcc. Or open the visual studio project in simulator/msvs. Let me know if you're having issues.
8) Some mixins are configurable from the designer (Like Draggable). They can be used manually in code as well.
9) Yes you can.
Don't apologize. I hope this answers your questions. I know some answers are brief, but i'd prefer if we dove into those individually if you say we should. The manual is more or less the knowledge based on touchgfx.zendesk.com, for now, until we can migrate to the ST documentation platform. You could check out the getting started tutorials, to get started.
https://touchgfx.zendesk.com/hc/en-us/categories/200529271
/Martin
2019-09-17 2:04 PM
Thanks , this is very helpful .
Will go more in depth as I progress :)
2019-09-18 3:41 AM
Looking forward to it :)
/Martin
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.