2019-03-08 1:33 AM
I'm getting errors (image attached) reporting that characters are not part of the typographics.
For both fonts reported i have a range of 0x20-0x7e entered for wildcard range (also shown in attached image)
Cant run simulator or target while in this mode, what am I missing?
2019-03-08 5:03 PM
Hi @brianshankland9,
Could you send me your project?
2019-03-11 3:04 AM
2019-03-11 3:36 AM
2019-03-11 3:56 AM
Just a quick observation (I haven't tried the project yet), but if you check out the first error in your screenshot, it looks like the text is really long (The end " is on a seperate line). Did you write this string directly in the designer or copy it from somewhere? The string could contain some special chars that actually aren't inside the font.
/Martin
2019-03-11 3:58 AM
I'm just getting a blank page on this dropbox share. How big is the project? You could reduce the size a bit by removing "touchgfx", "generated", "build" folders (I'll put the touchgfx folder there myself).
2019-03-11 4:11 AM
2019-03-11 4:13 AM
2019-03-11 4:18 AM
2019-03-14 4:21 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.