2026-04-03 2:35 AM
In TouchGFX 4.26.0 image order changes in application.config even if those images don't change.
This causes unnecessary changes to show up in git:
Feature request is to either preserve the order or to have them always lexicographically sorted.
2026-04-16 6:35 AM
Hello @unsigned_char_array ,
Thank you for reporting this issue. We were already aware of it and are working on a fix. It appears to be a regression compared with earlier versions, as a side effect of the improvements made to speed up TouchGFX code generation.
2026-05-04 11:06 AM
I had this for awhile.
If you are looking for which version as this regression.
My bet is when I passed from 4.25.0 to 4.26.0.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.