2025-07-02 2:24 AM - last edited on 2025-07-02 3:49 AM by mƎALLEm
I build a LCD driver board with STM32H750ZBT6 ,then i want to use built-in LTDC driver and SDRAM to run 480*270*16 TFT LCD panel , but touchGFX list following wrong message, where reason from ?
Generate Code
Generate
Done
Generate Assets
make -f simulator/gcc/Makefile assets -j8
0 [main] us 0 init_cheap: VirtualAlloc pointer is null, Win32 error 487
AllocationBase 0x0, BaseAddress 0x60EA0000, RegionSize 0x310000, State 0x10000
D:\TouchGFX\4.25.0\env\MinGW\msys\1.0\bin\sh.exe: *** Couldn't reserve space for cygwin's heap, Win32 error 0
simulator/gcc/Makefile:32: recipe for target 'assets' failed
make: *** [assets] Error 1
Failed
Failed
2025-07-02 4:19 AM
Hello @miker ,
You have an error when generating the assets but it seems to not be caused by TouchGFX but by cygwin or windows itself.
I found 2 great forum post that could help you :
Regards,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.