2019-05-18 7:56 AM
I've followed this article to configure a CubeMX project with TouchGFX graphics and IAR Embedded Workbench: https://touchgfx.zendesk.com/hc/en-us/articles/360019884752-Configuring-STM32F746G-DISCO
I got it working several times, but suddenly the linker gives an error:
Error[Lp011]: section placement failed
unable to allocate space for sections/blocks with a total estimated minimum size of 0x10'1d00 bytes (max align 0x4) in <[0x9000'0000-0x9010'0000]> (total uncommitted space 0x10'0001).
Error while running Linker
My application consists of a clock (made with this tutorial: https://touchgfx.zendesk.com/hc/en-us/articles/360018667192-Step-1-Setting-up-the-two-Screens) a using some hardware pins. (Blinking an LED and UART.)
All help is appreciated.
Solved! Go to Solution.
2019-05-18 12:44 PM
I removed alot of imagery from my gui, but forgot to delete them from the images tab in TouchGFX. After i did this, it works.
Thank You.
2019-05-18 11:17 AM
Should be 0x90000000..0x90FFFFFF
You can't cram more than 16MB (128Mb) into the QSPI, reduce the amount of graphic or imagery so it actually fits.
2019-05-18 12:44 PM
I removed alot of imagery from my gui, but forgot to delete them from the images tab in TouchGFX. After i did this, it works.
Thank You.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.