2023-07-21 8:18 AM
Hello, I have created a project to launch Touch GFX by stm32h723 , which I have put the download link below. Unfortunately, according to the photo I posted, it is displayed incorrectly on the LCD when it is launched, while I have separately tested the interface of the LCD and RAM, which work perfectly, but when I want to launch Touch GFX, I encounter this problem and it does not work.
link download project the onedrive
2023-07-21 10:36 AM
Hello
Try to move MX_TouchGFX_Process(); inside of default task loop. Now its called only once.
Br J.T
2023-07-21 1:35 PM
Thank you, I did this as well, but unfortunately it didn't have any effect. It's interesting that I previously got the correct answer with the stm32h743iit6 microcontroller with the same method, but I had a problem with the stm32h723zgt6!
2023-07-22 3:35 AM
OK. Anycase it should be called continuously, not just once.
Have you debug your code what does it do ? Does TouchGFX renders anything to the framebuffer ? Since you have solid background color, you framebuffer content should be mostly stable two values.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.