2019-03-25 4:25 AM
Hello,
I want to display the current time in TouchGFX project.
I am using TGFX 4.9.3 (using Keil IDE) and I want to use the Internal RTC to update set time.
The issue is that the clock settings are already defined when the project is created.
So I tried adding the required Clock Config (added in BoardConfiguration.cpp).
But it is not working.
Thanks,
Ameya
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.