2019-11-20 11:28 PM
Hi
I have a CustomContainer (menuScreen) that opens when pressing the menu button on my taskbar.
In the MenuClickHandler function the menuScreen is added and the following container appears:
By pressing a button the screen is being changed. The problem is when pressing on the white background it could happen that an interaction is triggered (e.g. button pressed) from the screen behind this container.
How can I set the entire screen behind the container inactive or not touchable?
Is there maybe another solution?
Regards Dejan
2019-11-29 1:06 AM
Taking a look now
2019-11-29 1:08 AM
The simulator doesn't compile through the designer.
There's a lot of headerfiles (probably target specific) being included from views. I tried fixing includes and code with #ifndef SIMULATOR but it's a bit too much work.
Could you fix the simulator to work? Generally, having target specific code in your views makes UI code non-portable. Something to consider.
The touch functionality should be the same from within the simulator as on target which allows us to inspect the problem.
Thanks.
/Martin
2019-11-29 1:26 AM
It's because I am including some header files from my main application.
I've never used the simulator.
I'm always testing on my hardware
If you just have a look in TaskBar.cpp (This is where I add the menuScreen) maybe you can see if I am doing something wrong.
Regards
Dejan
2019-11-29 1:39 AM
I'd rather try it - It's a lot more helpful and efficient for me to be able to debug the application. because from what you're describing you're not doing anything wrong.
Having a gdb-debuggable desktop application would be helpful for you as well to debug pure gui issues.
/Martin
2019-11-29 4:13 AM
To change the whole concept would need some time.
Do you have an example how to make the interface between target code and UI code?
Regards
Dejan
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.