2019-11-15 7:58 AM
With CubeMX 5.4 TouchGFX 4.12.3
I create a project from scratch on 32F746DISCO.
Generate code for IAR 8.32
And I have an linking error :
Error[Li005]: no definition for "MX_FREERTOS_Init()" [referenced from .......
Is it a bug or I miss something ?
2019-11-18 12:06 AM
Can you post the complete error log?
MX_* are methods created by CubeMX. Can you show me your main.cpp ? You shouldn't be missing something here, in my oppinion.
MX_FREERTOS_Init() is what creates the default task handle with the touchgfx main-event loop. It would appear that, for some reason, Core/src/freertos.c is not a part of your project. Can you confirm?
Did you enable the FreeRTOS IP in CubeMX?
/Martin
2019-11-18 12:53 AM
you shuild add "extern "c" " before MX_FREERTOS_Init().
2019-11-18 1:57 AM
The idea here is that the user shouldn't be required to do anything in order to achieve a compiling project - If extern "C" is missing and freertos.c is actually being compiled then we may have found an issue.
/Martin
2019-11-18 7:20 AM
I think I found why :
You can reproduce it by validate "Generate peripheral initialization as a pair of '.c/.h' files per peripheral in generated files in project manager of STM32CubeMX project.
Is I devalidate this option, I have mo more this error
Let me know if you can reproduce it
2019-11-18 8:16 AM
I can reproduce the problem in CubeIDE 1.1.0 The project was created using the integrated CubeMX-tool.
I found the problem only occurs when I activate the GRAPHICS Middleware in the setup tool and the "Generate peripheral initialization as a pair of '.c/.h' files per peripheral". If either is deactivated everything seems fine.
I also tried adding "extern "c" before MX_FREERTOS_Init() but this just leads to more errors inside freertos.c.
Best regards
Christoph
2019-11-20 5:14 PM
Hi,
Martin, are you able to reproduce it and do you find the bug ?
Thanks
Sébastien
2019-11-24 3:55 PM
Please any feedback about this.
Is it a bug a I made something wrong ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.