cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX 5.0.1 Empty hal_conf file on 32F746DISCOVERY demo

MEder
Associate III

I am attempting to ​setup the TouchGFX on a 32F746DISCOVERY Board with CubeMX and SW4STM32.

When I create the Board project in CubeMX, the stm32f7xx_hal_conf is empty.

I would have expected that the Peripherals would have some initialization code setup by Cube, but I am new to Cube so perhaps someone can point out if stm32f7xx_hal_conf needs to be setup by me or if its a bug in Cube.

Thanks

Martin 

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
MEder
Associate III

​Hello,

OK, I have resolved this issue on Win 7. 

I uninstalled Cube,

Re-installed JRE,

Installed CubeMx.

Now, I get a populated stm32f7xx_hal_conf.h file.   

Thanks

View solution in original post

3 REPLIES 3
Imen.D
ST Employee

Hello,

Please share your ioc file for check.

Kind Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

​Hi,

I think this is a JRE Problem. I am running Win7, and JRE 1.8.201.

On a Win X system I can Create the project and get a correct hal_conf file.

Thanks

MEder
Associate III

​Hello,

OK, I have resolved this issue on Win 7. 

I uninstalled Cube,

Re-installed JRE,

Installed CubeMx.

Now, I get a populated stm32f7xx_hal_conf.h file.   

Thanks

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.