2020-10-09 10:55 AM
Hello, I am having some difficulty implementing a screen transition. I have followed along this thread, but it seems there are some underlying issues with MVPApplication that are not allowing a template arguments to deduced/substituted.
Versions:
TouchGFX 4.13.0
STM32CubeIDE 1.2.0
I have a screen transition that I created from within TouchGFX Designer that works perfectly fine, but it requires me to have a button that I don't actually need on the screen. I would like to create my own screen transition that I can use from code. So I used the TouchGFX Desginer generated code as a template, and then deleted the interaction in TouchGFX Designer once I had copied the code.
What I have so far...
If my FrontendApplication.cpp file I have added this code:
#include <mvp/MVPApplication.hpp>
#include <gui/datetime_screen/DateTimeView.hpp>
#include <gui/datetime_screen/DateTimePresenter.hpp>
void FrontendApplication::gotoDateTimeScreenSlideTransitionEast()
{
transitionCallbackTwo = touchgfx::Callback<FrontendApplication>(this, &FrontendApplication::gotoDateTimeScreenSlideTransitionEastImpl);
pendingScreenTransitionCallback = &transitionCallbackTwo;
}
void FrontendApplication::gotoDateTimeScreenSlideTransitionEastImpl()
{
touchgfx::makeTransition<DateTimeView, DateTimePresenter, touchgfx::SlideTransition<EAST>, Model >(¤tScreen, ¤tPresenter, frontendHeap, ¤tTransition, &model);
}Now when I compile the code I get the following errors:
In file included from ../TouchGFX/generated/gui_generated/include/gui_generated/common/FrontendApplicationBase.hpp:7:0,
from ../TouchGFX/gui/include/gui/common/FrontendApplication.hpp:4,
from ../TouchGFX/gui/src/common/FrontendApplication.cpp:1:
../Middlewares/ST/touchgfx/framework/include/mvp/MVPApplication.hpp:192:16: note: candidate: template<class ScreenType, class PresenterType, class TransType, class ModelType> PresenterType* touchgfx::makeTransition(touchgfx::Screen**, touchgfx::Presenter**, touchgfx::MVPHeap&, touchgfx::Transition**, ModelType*)
PresenterType* makeTransition(Screen** currentScreen, Presenter** currentPresenter, MVPHeap& heap, Transition** currentTrans, ModelType* model)
^~~~~~~~~~~~~~
../Middlewares/ST/touchgfx/framework/include/mvp/MVPApplication.hpp:192:16: note: template argument deduction/substitution failed:
../TouchGFX/gui/src/common/FrontendApplication.cpp:121:139: note: cannot convert '((FrontendApplication*)this)->FrontendApplication::<anonymous>.FrontendApplicationBase::frontendHeap' (type 'FrontendHeap') to type 'touchgfx::MVPHeap&'
touchgfx::makeTransition<DateTimeView, DateTimePresenter, touchgfx::SlideTransition<EAST>, Model >(¤tScreen, ¤tPresenter, frontendHeap, ¤tTransition, &model);
^~~~~~~~~~~~
make[1]: *** [TouchGFX/gui/src/common/subdir.mk:18: TouchGFX/gui/src/common/FrontendApplication.o] Error 1
make[1]: *** Waiting for unfinished jobs....
make: *** [makefile:105: all] Error 2
"make -j all" terminated with exit code 2. Build might be incomplete.
2020-10-12 1:48 PM
Hello Jhard.17,
I'm going to answer tomorrow because i've already done that but my code is on my PC at my work office.
Regards,
AJT141
[EDIT] : so here is my anwser
Imagine you want to create a transition to go to s_resident_name screen.
You have to add this in "FrontendApplication.hpp" :
You have to implement these functions in "FrontendApplication.hpp" :
void FrontendApplication::gotoscreenResidentScreenNoTransition()
{
own_transitionCallback = touchgfx::Callback<FrontendApplication>(this, &FrontendApplication::gotoscreenResidentScreenNoTransitionImpl);
pendingScreenTransitionCallback = &own_transitionCallback;
}
void FrontendApplication::gotoscreenResidentScreenNoTransitionImpl()
{
touchgfx::makeTransition<s_resident_nameView, s_resident_namePresenter, touchgfx::NoTransition, Model >(¤tScreen, ¤tPresenter, frontendHeap, ¤tTransition, &model);
}And you need to add the initialization of own_transitionCallback in FrontendApplication constructor :
FrontendApplication::FrontendApplication(Model& m, FrontendHeap& heap)
: FrontendApplicationBase(m, heap), own_transitionCallback()
{
}Now, if you want to switch to resident Screen you just have to call gotoscreenResidentScreenNoTransition like that :
application().gotoscreenCommunicationEstablishedScreenNoTransition();Did you forget to include that ?
#include <touchgfx/transitions/slideTransition.hpp>
2020-10-12 5:46 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.