2021-05-12 10:17 AM
Is it possible to create a costum container with a TextArea, which hast a variable ResourceID. I want to create a template for a MenuItem.
When using a costum container i had to create a new costum container for each specific Text/ResourceID, right?
A costum widget could be a solution i guess, but this only can be done by code.
Will it be possible in the near future to create and use Costom Widgets in the TouchGFX Designer?
2021-05-16 7:56 PM
Hello MAu,
(If I understand correctly your question) Custom Containers can definitely have a TextArea. Plus this TextArea can be changed accordingly as a MenuItem. For this, the TextArea needs to use Wildcards.
Also, Custom Containers can already be used in Designer. If you are talking about not using Custom Containers as a MenuItem but normal widget, you will find your created CustomContainer in the list of widgets when clicking on the (+) [Add a widget].
Please have a look at the UI Example "Scroll Wheel and Scroll List" available in TouchGFX Designer.
/Alexandre
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.