2025-01-30 9:30 AM - last edited on 2025-02-10 8:03 AM by Andrew Neil
I am using a Rivierdi display with their board that uses a STM32H757XIH6. I am using touchgfx and starting with their pre-made example in touchGFX. Their board has a 40 pin connector that give access to I/O. I am using their project as a starting point and trying to change I/O functions to simple GPIO from alternate function however when I make this change, the project ceases to build. Here is a specific example:
I changed PD11 to GPIO output from LPTIM2_IN2 using pinout view:
I then generated code in CubeMX and tried to build the new project in CubeIDE. The project built fine before the change but failed after this with the following error:
make: *** No rule to make target 'C:/TouchGFXProjects/Regal_shutoff/CM7/Core/Src/lptim.c', needed by 'Application/User/Core/lptim.o'. Stop.
What do I need to do to clear this?
Solved! Go to Solution.
2025-01-30 10:38 AM - edited 2025-01-30 10:42 AM
Hello @TIF ,
I think these posts may help you:
Solved: make[3]: *** No rule to make target 'CM7/TouchGFX/... - STMicroelectronics Community
No rule to make target 'TouchGFX/build/STM32H750B-... - Page 2 - STMicroelectronics Community
2025-01-30 10:38 AM - edited 2025-01-30 10:42 AM
Hello @TIF ,
I think these posts may help you:
Solved: make[3]: *** No rule to make target 'CM7/TouchGFX/... - STMicroelectronics Community
No rule to make target 'TouchGFX/build/STM32H750B-... - Page 2 - STMicroelectronics Community
2025-02-10 7:48 AM
Thank you! I was hoping to not have to manually manipulate those as I worry that I may break something that is used by demo board.
One thing I noticed is using the external CubeMX application caused issues but using the CubeMX integrated in CubeIDE seemed to work much better.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.