2020-08-31 6:19 AM
I want to uncomment #define SINGLE_FRAME_BUFFER_INTERNAL to use single frame buffer in internal SRAM and i dont want TouchGFX to generate codes about FMC. Where exactly BoardConfiguration.cpp generated.
Solved! Go to Solution.
2020-08-31 8:07 AM
We don't use that define with the Generator. It was mostly for BoardConfiguration.cpp's that could handle both double and single. TouchGFX Generator just calls setFrameBufferStartAddresses with one, two or three arguments. And in the case of single FB we use a specific framebuffer strategy.
/Martin
2020-08-31 6:30 AM
@Martin KJELDSEN can you help?
2020-08-31 6:55 AM
How did you generate the project? If through TouchGFX Generator / CubeMX then it's not called BoardConfiguration anymore, but TouchGFXConfiguration.cpp and its located in the TouchGFX/target/generated/ folder.
The define is there because you chose SINGLE Framebuffer in the generator (if you did) and you can just choose something else.
/Martin
2020-08-31 7:44 AM
Well i started the project on TouchGFX, created my GUI and generated to code to open the project from .project file with STM32CubeIDE. From the CubeMX i changed the Double Frame option to single But i couldnt find the #define SINGLE_FRAME_BUFFER_INTERNAL in TouchGFXConfiguration.cpp. Do suggest me to start project from CubeMX perspective and import to CubeIDE and lastly add GUI from .part file from scratch?
2020-08-31 8:07 AM
We don't use that define with the Generator. It was mostly for BoardConfiguration.cpp's that could handle both double and single. TouchGFX Generator just calls setFrameBufferStartAddresses with one, two or three arguments. And in the case of single FB we use a specific framebuffer strategy.
/Martin
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.