2021-06-06 11:32 PM
So in TouchGFX designer, when we choose Dynamic Graph widget, we can input the number of data points. Let's say originally we set as 100 data points, but later we want to increase this, can we do this?
Also, is it really possible to increase X axis range without increasing the data point?
2021-06-07 12:15 AM
Look at sources of Graph and you will see that there is no such functionality. Data is stored in an array of fixed length.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.