2020-02-12 1:51 PM
I'm interested in using the Nucleo StmH7 with the L6474 X-NUCLEO-IHM01A1 board.
However I'd like to run STSW-SPIN002 to communicate with it, but that expects to talk to the NUCLEO-F401RE... so I need the protocol that's implemented in order to port to the NUCLEO-H743ZI.
Is it possible to get the source code for Guifw-STM32F4xx-Nucleo.bin?
2020-02-17 1:45 AM
It doesn't sound like it's TouchGFX running on that board, so its definitely not something we've done here at the office. I'll try asking around.
/Martin
2020-03-18 9:04 AM
If the source code that runs on the Nucleo cannot be open-sourced (to be ported to the Nucleo H743ZI) , what about source code for the other side.. the PC software STSW-SPIN002 that talks to it?
If neither, how difficult would implementing the motor movement protocol based on just analyzing the serial traffic between the PC SPIN and the Nucleo F401RE?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.