2023-08-03 6:44 AM
Hello everyone
Can I also add an svg image to a button? I can embed images in svg format (almost) without any problems. However, if I want to assign an image to a flex button, only png works. Is there a workaround for this or does it just not work?
Regards, Roger
Solved! Go to Solution.
2023-09-21 4:53 AM
Hello @Roger.ch ,
Unfortunately, SVGs are not supported on buttons yet. You can only use SVG as standalones.
However, you can use an 'SVG Image' and then enable ClickListener option for it under the Mixins section. This way you can have the click functionality of a button, and you can manually (I mean from the code) set different SVGs for different click events (but it might be a bit tricky to handle perfectly) to imitate Released or Clicked states.
Good luck
2023-09-21 4:53 AM
Hello @Roger.ch ,
Unfortunately, SVGs are not supported on buttons yet. You can only use SVG as standalones.
However, you can use an 'SVG Image' and then enable ClickListener option for it under the Mixins section. This way you can have the click functionality of a button, and you can manually (I mean from the code) set different SVGs for different click events (but it might be a bit tricky to handle perfectly) to imitate Released or Clicked states.
Good luck
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.