2020-06-02 5:20 AM
Hi,
I set the binary option in the designer (4.13) and successfully generated the bin files. I then unset the option and generate again the fonts fileד. All this session worked as expected.
Now, after a while, in the same project, I set the binary option again but this time the bin directory was not created.
Any idea?
Thanks
2020-06-02 5:30 AM
Are you sure it wasn't just deleted? Using binary fonts is a bit convoluted at the moment and we're working on a better solution - We've got a script that can generate glyphs without using the excel sheet. When you uncheck the "binary" option you need to store the generated bin file before re-generating.
2020-06-02 12:18 PM
Since the project includes various fonts and only one of the fonts need to be use as a cached binary font we did the following:
Now, in that stage, if I want to repeat the process, maybe with another font from the project, and I set the binary font option and generate I can't get the bin directory again any more.
2020-06-03 3:47 AM
Okay, i'll try out your flow when i can! Thanks
/Martin
2020-08-18 5:55 AM
Hi Martin,
In another 4.13 project that is up and running without binary option set I need to add the binary font option.
I set the binary fonts option in the designer, generated the code rebuild and the bin directory is created but it is empty, any idea what could be wrong?
Thanks,
Eyal
2020-08-18 6:02 AM
I can see that if the bin directory exist the binary fonts are created into it
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.