STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

DCMI DMA synchronization on STM32F7

Posted on June 06, 2016 at 19:52I have the STM32F746 Discovery board and my project works with the OV9655 camera. I am trying to switch over to use the MT9V034 camera chip from Aptina/OnSemi, which outputs 8bit grayscale (really, it outputs 10bit, b...

wflanery by Associate II
  • 1439 Views
  • 1 replies
  • 0 kudos

DMA2D / Chrom-ART questions

Posted on March 11, 2016 at 10:49Hi, I'm trying to use an STM32F4 to render images on a display using DMA2D. I'm fairly new to graphics and blending so I would appreciate some input. Say I'm trying to display two 100x100 squares, one red at 0,0 and ...

aditya23 by Associate II
  • 1076 Views
  • 1 replies
  • 0 kudos

Flickering Display

Posted on March 22, 2016 at 15:40I'm using DMA2D to draw images on the display. I'm using two layers and both of them will eventually be animated. But at this time I'm trying to move just one object on one layer around the screen, but the entire dis...

aditya23 by Associate II
  • 1165 Views
  • 1 replies
  • 0 kudos

STM32F7 TFT with LTDC and DMA2D

Posted on May 04, 2016 at 11:06Hello everybody, I am trying to understand how the LTDC and DMA2D are working together. I have a small custom made STM32F7 board with a 24-Bit RGB TFT panel connected to the LTDC. With CubeMX I activated this interface...

dennis23 by Associate II
  • 2713 Views
  • 3 replies
  • 0 kudos

Missed GUIDRV_SLin support in STemWin

Posted on March 31, 2016 at 11:16I need to use STM32F4 to control a LCD with RA8835 controller on it. By the document given with STemWin, I need to call GUIDRV_SLin_SetS1D13700(). But in ARM MDK, it always throw error ''Error: L6218E: Undefined symb...

STemWin ST32F429

Posted on April 27, 2016 at 11:46I downloaded stm32cubef4.zip and tried to build a STemWin test application from the emWin files included.  The builder complained something about C:\Users\bennacef\Desktop\SVN\STM32_emWin_Library.  What is this benna...

emWin and CubeMX 4.14

Posted on April 26, 2016 at 21:56I am trying to create an STemWin application for STM32F429 discovery.  I have an old application, handmade from some old CubeMX.  It is working fine.  Now I created a new basic project with CubeMX 4.14, I only select...

LTDC Moving Layer (scroll effect)

Posted on April 22, 2016 at 20:26Hello!I'm trying to use the peripheral LTDC to move the layer.I'm loading an image 1024x768 at address 0xD0000000 SDRAM.I need to move the display layer that has the resolution of 240x320, it is necessary to make a s...

Unable to link emWin - missing LCD_IO_WriteReg

Posted on April 07, 2016 at 13:15I'm trying to build a first graphical LCD project with Visual GDB (which lets you use Visual Studio for embedded development using the ARM GCC toolchain). I can't find any sign of any of the LCD_IO_ routines in the ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.