STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! STM32F746G-DISCO Display datasheet

Posted on September 16, 2016 at 22:11Hello, I really need the STM32F746G-DISCO display (RK043FN48H-CT672B) datasheet. (Not only source code of CubeMX firmware) I contact ROCKTECH and ST without success. Can someone send me this datasheet ? Thanks in...

STM32F429i_Discovery with LCD load logo or image

Posted on September 15, 2016 at 10:10Hello everyone, I hope you are well. I have a small problem I would like to display a logo of my my university on board STM32F429i_Discovery but I sometimes displaying the logo ST. I use LCD image converter but ...

ibrahim by Associate II
  • 9223 Views
  • 29 replies
  • 0 kudos

STM32F429 100pin TFT Drive

Posted on August 22, 2016 at 08:16HiI'm trying to use STM32F429 to drive TFT LCD and want to use it without any driver chip directly by the micro pins. As I checked, some pins are missing in 100pin package such as LCD_R0, LCD_G1, LCD_G2, LCD_B0, LCD...

_behn4m by Associate II
  • 2092 Views
  • 3 replies
  • 1 kudos

Question for LCD Blink feature.

Posted on August 30, 2016 at 01:18I'm using STM32L073 with LCD glass module.The LCD glass has 27 segments, 1/3 bias.I'm going to blink up to specific pixels(seg10, com3) using the BLINK bits in the LCD_FCR register.In reference manual, Blink mode ha...

ubcho by Associate
  • 1311 Views
  • 1 replies
  • 0 kudos

STemWIN + SDRAM + LTDC

Posted on June 20, 2016 at 19:57Hello, I use a STM32F429 Discovery board with an other Display (Newheaven 800x480,7 incheshttp://www.newhavendisplay.com/nhd70800480efatxvctp-p-6912.htmlI use the LTDC controller of the STM32F4 to control the display....

0690X00000603FTQAY.jpg 0690X00000605YSQAY.png

emWin: Problem with STM32F746 Disco board

Posted on August 20, 2016 at 17:48HelloI have a STM32F429I-Eval boardand a STM32F746 Disco board.I want to use StemWin with the GuiBuilder.On both Boards I use the ''Hello World'' Examples as templates.On the STM32F429I-Eval the Dialog are shown cor...

0690X00000603BVQAY.jpg 0690X00000605OTQAY.png 0690X00000603CYQAY.jpg
mfrank9 by Associate III
  • 1458 Views
  • 3 replies
  • 0 kudos

Where is the Graphics Library in ST32M CubeMX ?

Posted on August 21, 2016 at 14:34I m New to STM32 and TFT. I need to Interface a TFT LCD with Touch screen to ST32103CB MCU. Which is the library or example project ST Micro provides for this task for me to begin as a template. The example I found ...

roythomas by Associate II
  • 1174 Views
  • 1 replies
  • 0 kudos

STemWin & ili9341 driver

Posted on July 22, 2016 at 11:39Hi,I have been successful in getting a project running on a STM32F746-Nucleo-144 board and now want to add an LCD to it. I bought a 2.4 inch Arduino shield with ili9341 driver and 8 bit parallel connector as it fits n...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.