STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Image processing on the STM32F7?

I have an OpenCV image processing application running with a Raspberry Pi, but it's overpowered for my needs, so I'm exploring options for getting my project running on something slower and cheaper. The STM32F7 seems to hit the mark as far as process...

ukn by Associate
  • 1043 Views
  • 0 replies
  • 0 kudos

Resolved! CubeMX + STEmWin + Atollic Integration ETA

Posted on May 28, 2018 at 17:56Project generation in CubeMX is great. Atollic now that it is free is great. STEmWin is.... ok. I'd like to generate STemWin based projects with CubeMX while using the Atollic IDE. As some of you might know, when you E...

0690X0000060BP6QAM.png

I want Layer Copy. Help me.

Hi.I am using the virtual layer to display the screen on the lcd.I am trying to copy between virtual layers.RGB 16BIT is used and the resolution is 480 * 800.I want to copy the screen at (0,0) to (0,800), but it does not work normally.ex)GUI_CopyRect...

STM32F1 discovery programming with Arduino

I am trying to use arduino IDE to program the STM32F1 discovery with waveshare 4inch LCD using the demo code provided https://www.waveshare.com/wiki/4inch_TFT_Touch_Shieldam I using the correct package?https://github.com/stm32duino/BoardManagerFiles/...

hhuyn.6 by Associate
  • 1645 Views
  • 1 replies
  • 0 kudos

HOW USE CUBEMX HAL_LCD_WRITE?

It is the starter that started now. We are currently using the STM32L152C-DISCOVERY board.I have used HAL_LCD_WRITE as shown below, but nothing is displayed on the LCD.HAL_LCD_WRITE (& hlcd, LCD_RAM_REGISTER0, 0x0000, 0xffff);orHAL_LCD_WRITE (& hlcd,...

ngabj by Associate
  • 1544 Views
  • 0 replies
  • 0 kudos

STM32H7 Cache configuration for USB HS

How do I need to configure cache validation invalidation for USB transfer to PC of continuously DMA filling buffer? Right now I have some visible errors ( I stream DCMI video via USB).

esukh by Associate III
  • 806 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.