STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Help FATFS

So i need to use a filesystem to use the qspi flash on my stm32f769 disc board and once i have all the code ready, all i get are "defined but not used" and "previously defined" errorsHow can i suppress these?

pmppires by Associate II
  • 2560 Views
  • 5 replies
  • 1 kudos

Printing font on ST7735 ?

Dear Members,I tried to print string on ST7735ST7735_WriteString(0, 0, "Font_7x10, red on black, lorem ipsum dolor sit amet", Font_7x10_ST7735, ST7735_RED, ST7735_BLACK);but I got only white screen, I saw on my debug Font_7x10_ST7735 data = 0 buton t...

Running the TouchGFX project out of the box

I downloaded the IAR IDE and installed it, selecting the time-limited license so there isn't a limit on code size.I downloaded STM32Cube_FW_F7_V1.15.0 and unzipped it.I double-clicked on the Project.eww file in the STM32F769I-Discovery/Demonstrations...

MPlan.7 by Associate III
  • 819 Views
  • 0 replies
  • 0 kudos

STM32F429-DISC1 White Screen Error

Hello , I just bought STM32F429-DISC1 a few weeks ago.I did the following :Turned it ON by connecting to my laptop.installed the drivers. and updated the firmware Everything worked perfectly fine. Then I put it in a box safely because I was busy with...

0690X00000895hFQAQ.jpg

Access a scrollable container using hard keys

Hi, I want to access a scrollable container using Hard keys, is it possible? I have tried with doscroll virtual function by creating a subclass for scrollable container. We are using LCD with no touch option, so i have to control the scrollable conta...

PBU by Associate III
  • 777 Views
  • 1 replies
  • 0 kudos

Resolved! Are there in-depth ways to investigate why HAL_DCMI_Start_DMA() is not putting data into the"*pdata" pixel buffer?

I am getting pixel data to the stm32. I am reaching the "end of frame flag clearing" at:stm32l4xx_hal_dcmi.c ----> HAL_DCMI_IRQHandler() ----> (line 811)__HAL_DCMI_CLEAR_FLAG(hdcmi, DCMI_FLAG_FRAMERI);I am simply checking cameraBuffer[] pixel array u...

KM.8 by Associate III
  • 27002 Views
  • 11 replies
  • 0 kudos

Touch Gfx and Keil uVision

I try to use my STM32F429 Discovery Kit with: Touch Gfx and Keil uVision.I’m able to create a program with STM32CubeMX ( follow this guide:https://touchgfx.zendesk.com/hc/en-us/articles/360021620431-Configuring-STM32F429I-DISCO )but I have some probl...

GPinz by Associate
  • 1774 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.