STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

STM32L DSI rxclkesc

Hello,I have 32L4R9IDISCOVERY board with round display. When I set clock configuration of MIPI DSI there is one error. DSI rxclkesc is same as DSI lane byte clock if lane_byte_clock is fed from DSI-PHY. For 32F469IDISCOVERY DSI clock setting there is...

0690X000008AJjAQAW.png

How to use Callback in touchgfx

Hello all,I am trying to configure a click event upon a scrollwheel for selecting an item.I am using Callback for achieving this.Inside a handleClickEvent(), I need to give a callback to a CallbackHandler function. This function will eventually call ...

kvkhekale by Associate II
  • 3701 Views
  • 3 replies
  • 0 kudos

Resolved! Program control reaching handleClickEvent, instead of handleDragEvent, upon drag action on touchscreen

Hello,I am configuring ScrollWheel on touchgfx.In order to select an option, I need to click on ScrollWheel.In order to browse all the options, I need to drag on ScrollWheel. So, I need both handleClickEvent() and handleDragEvent(). I also need to d...

kvkhekale by Associate II
  • 4264 Views
  • 5 replies
  • 0 kudos

i got touchgfx + uart interrupt problem.

Hi.I am using the uart on the touchgfx project on the stm32f746-disco board, but when I continue the uart interrupts, I get stuck.There were two cases of stuck state.1. Screen stops but uart is running2. Board is completely frozenThe uart interrupt c...

0690X0000088PuvQAE.png 0690X0000088PulQAE.png 0690X0000088PugQAE.png 0690X0000088PubQAE.png
YJMoon by Associate III
  • 5465 Views
  • 10 replies
  • 0 kudos

stm32f767 hardware jpeg decode header all zeros

Porting the basic JPEG_DecodingUsingFs_DMA from Discovery to custom hardware and I'm failing with the hardware JPEG decoder. The image decodes fine with the software decoder in STemWin and although I seem to be getting the HAL_JPEG_IRQHandler interru...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.