STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

When will STM32CubeIDE support TouchGFX ?

For now, STM32CubeIDE have an option to enable TouchGFX. However it does not compile after code generating. I tried to solve the problems but I have not succeeded for the moment (using STM32F746G DISCO, C++). For information, I saw and followed the g...

Resolved! Creating a new task for HW interaction

Hello,I'm trying to extend the example given in 'Method 2 - From other task', given here: https://touchgfx.zendesk.com/hc/en-us/articles/205074561-Connecting-the-UI-to-your-systemI am using the 746-Disco board and the example works just fine on my ha...

HP by Senior III
  • 2089 Views
  • 8 replies
  • 0 kudos

Resolved! Designer Run Simulator error!

I used cubemx to generate the project, using designer generate gui code. This project works well in VS, MDK and development boards.But use run simulator in designer to prompt the errors shown in the figure.Excuse me, where did this go wrong, how shou...

0690X000009878ZQAQ.png
lxw by Senior
  • 4516 Views
  • 10 replies
  • 0 kudos

The content of snapshot widget is wrong.

Hi,Now My Platform setup is as following,custom boardtouchgfx 4.10.0IAR 8I'm trying to use snapshot widget in my project. I did the following configuration,In setFramebufferAddress function, set Animation storage to true.create a snapshot widget obje...

L4Y by Associate II
  • 1691 Views
  • 3 replies
  • 0 kudos

How to handle DMA2D Transfer Error

Hi,I'm working with touchgfx on an STM32F769I board and I'm facing a problem where some times the DMA2D throws a transfer error (DMA2D_ISR_TEIF) during the running of my application. In the touchgfx library files (STM32F7HAL_DSI.cpp) I see that the D...

Nikil Rao by Associate II
  • 4237 Views
  • 8 replies
  • 0 kudos

Resolved! Problems upgrading from 4.9.6 to 4.10.0

Hi @Martin KJELDSEN​ !You usually support me with TouchGFX, this must be a simple one for you but I can't find the solution in the community.I'm having an issue trying to update my project from TouchGFX 4.9.6 to 4.10. I get the build error:undefined ...

problem with the tm_stm32_lcd.h

hi ST Community,in the pic below, there's a problem with the file.h indeed I've included the file as shown.can someone give me a solution? or maybe you've seen this before.Thanks

0690X000009883VQAQ.png 0690X000009883BQAQ.png 0690X000009882rQAA.png
idrissmc by Associate III
  • 742 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.